Posted on May 17, 2011 at 11:32I confirm that, from my experience, using a ST92F120-EPB without adding the two Voltage Regulator Stabilization capacitors does not limit the ST92F150 read/write/erase features.
Posted on May 17, 2011 at 10:16Hello Please find here below the answer to your questions: 1: There is no option byte to protect the device in the ST72141. In Fact there is no option bit at all. 2: Normally, you cannot do ISP with ST72141 but try it ...
Posted on September 24, 2002 at 14:17The ST10F269 includes an internal 256Kbyte FLASH memory and 12 Kbytes of RAM. This memory can be extended up to 16Mbytes with an external memory device (5Mbytes if CAN is used).