Posted on May 17, 2011 at 10:15Thank for you advise on FOCgui which seem very interesting, but i'm not sure i can use it with my ST7(because of 8bit micro instead of 32bit). Perhaps i can check for buying such platform i there no other solution. I n...
Posted on May 17, 2011 at 10:15Thank a lot for your rapid answer, which encourages me a little bit. The phase resistance is 5.5 Ohms per phase. I agree that the electrical spec are very poor. I guess Inductance could be also usefull, but as the freq...
Posted on May 17, 2011 at 10:15We are using a 1,8 kW Ginlong Permanent Magnet Generator. It is three phased and has 16 poles. The voltage can reach 500 V at 600 RPM. Since we are designing a Vertical axis wind turbine, we need to start it thanks to ...