Posted on October 27, 2016 at 09:10
Hello,
I ported the microchip MiWi stack to STM32(NucleoL152RE) initaly using the mbed hardware librarys. I do not use the mbed compiler, but rather imported it into EmBitz and use the arm-none-eabi...
Posted on October 27, 2016 at 13:06Hello,yes, as I mentioned already, I ported all the function from the mbed and HAL drivers to the SPL. I find it hard to debug at the moment, as there is no clear fault, besides the fact that only the hardware acce...