Posted on October 07, 2016 at 11:17
Hello, I have problem with stm32f373 ADC peripheral. My config ADC1 pin PA2 always gives 1.6 V at output, but it's configured as analog input. I usedADC_BasicExample, but result is the same. In errata no infor...
Posted on October 18, 2016 at 19:23Hello Mayla, Yes, I have tried with another channel, but still the same voltage offset on all of the channels.When ADC clock disabled, there is approximately 68-70 mV, so I suspect its correct. These channels input...