User Activity

Posted on October 07, 2016 at 09:40
Posted on October 04, 2016 at 15:01 Hello. After the initialization CAN interface and call HAL_CAN_Receive_IT function (& hcan, CAN_FIFO0) there is no interruption USB_LP_CAN_RX0_IRQ Handler (); when receiving the CAN package. And accordingly mi...
Posted on September 06, 2016 at 18:15http://www.compel.ru/infosheet/ST/STM32F302R6T6STM32F302 CAN and USB at the same time?We are thinking of using an STM32F302R6T6  KB for our next project. But I need to know if CAN and USB can be used at the same ...