This was the problem, that the behavior is not mentioned in the datasheet. You can only measure it. I had the same problem if you can read, then my answer below will confirm the behavior which mattwo has found.
Posted on April 05, 2017 at 15:36Yes i am sure.For static addresses it is right that only 2 sensors can be used at one IIC bus. But if you connect the SDO/SA1 pin of the sensor to a GPIO pin of the MCU you can switch dynamically the addresses and wi...
Posted on September 07, 2016 at 13:48hello matt, thank you very much for your post. I had the same problem, 4 LIS3MDL connected at one IIC interface. I used the SDO/SA1 line for adress selection (with low-state in standby) and current was around 450...