Posted on April 19, 2016 at 14:32Hello,when setting such a low output voltage value I suggest to use X version (30kHz) instead of L, in order to avoid that, due to the large input to output difference, the Ton required to keep the output under regul...
Posted on April 04, 2016 at 16:41Hello,Vdd shorted to ground probably means that the pin has been forced to a current/voltage value higher than its absolute maximum rating (AMR).This event cannot be ascribed to e-design studio, since several checks ...