Hi everybodyI'm trying the Tutorial 3 of touchgfx documentation because I have to evaluate touchgfx against another graphic framework.BOARD: STM32H7B3I-DKTouchGfx designer 4.13.0Project created by designer using the board template.On PC simulator eve...
Posted on March 25, 2016 at 22:29 The original post was too long to process during our migration. Please click on the attachment to read the original post.
Hi MartinI attached the project in 7z instead o zip, it was half the size. The simulator is going fine, for hours. I speed up the circle clock speed, in this way it happens fast the problem, just few seconds. I have only change the arc start and arc ...
Hi MartinI have checked, the Canvas buffer was 7200... I increased the buffer overriding the size to 32767 as max possible value. The problem still persist the same call stack. No frame are rendered (the blu led of the board is not flashing anymore)....