2009-04-30 01:48 AM
What's matter about EMI of stm8a?
2011-05-17 06:03 AM
Hello
I use finger touch crystal pin, The programm do not go on normally. This can be Forgiven... But when I left finger ... Poweroff ... Poweron again ... I find the program run away...God save me! I must programm it again to restore Why?! Regards wolver2011-05-17 06:03 AM
Hi Wolver,
STM8A follows the standard EMC compliancy tests needed for the automotive devices. Could you explain your test in more details? Do you have de-coupling capacitors present on all the power supply pins? As you said below, the program runs away, do you mean that the program memory is blank or it is corrupted? Which STM8A device, you are using? BTW, what project you are working on with STM8A. Are you a ST customer or working inside ST ABU? Regards, Jatin2011-05-17 06:03 AM
Hi Jatin
en... 1. I have de-coupling capacitors present on all the power supply pins. You can seehttp://www.st.com/mcu/modules/Splatt_Forums/downloadtemp/MCU_Block___01_STM8AH5188.pdf
2. 'program runs away' means' flash was changed and programm did not go on.. 3. The project use STM8AH51A8, That is designed for the car of model B50 which produced by FAW-VW Automobile Co., Ltd. in China(http://www.faw-vw.com) 4. I am ST customer... 5. This question more details is reported to ST FAE(joyce.yan@st.commailto:sherry.li@st.com
mailto:zhao-yi.li@st.com
) ShanHai & Beijing in China., Since I am not good at writing English... This question must be checked out and resolved... otherwise, STM8A will be say good by for this automotive project... Regards wolver2011-05-17 06:03 AM
Thanks Wolver for the below info.
No problem, I will get the problem details from Joyce Yan. For sure, we will help to understand and resolve this problem. Regards, Jatin2011-05-17 06:03 AM
Hi Jatin
Thanks for help! Attention please ... This question will be resolved deadline is 2009-5-15. If not, I will say sorry about STM8A ... Regards wolver2011-05-17 06:03 AM
I have alreay asked Joyce Yan about the problem details.
Few questions: 1. Are you writing program memory in your code? 2. Unused memory location are filled with trap instruction or not? 3. What portion of program memory is changed ? You can also have a look at the app note AN2860. There are some other AN's suggested inside this AN.2011-05-17 06:03 AM
Hi Jatin
1. Are you writing program memory in your code? A: No, You can check my source code from Joyce Yan 2. Unused memory location are filled with trap instruction or not? A: No, I have not filled with trap instruction, But I will try it according to Joyce Yan's mail... 3. What portion of program memory is changed ? A: I have mailed all informatios to Joyce Yan. please contact her. Regards wolver2011-05-17 06:03 AM
Hi Jatin
Where is app note AN2860? Regards wolver2011-05-17 06:03 AM
Hi Wolver,
Please find below the link: http://www.st.com/stonline/products/literature/an/15267.pdf Regards mozra