cancel
Showing results for 
Search instead for 
Did you mean: 

wakeup function

SRAM.11
Associate III

How to use Port D as wake up function after the STMS003

goes to sleep

 

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
AA1
Senior III

You have to configure a pin to generate and interrupt and you need the interrupt handler. See RM0016 "External interrupts" and "Power management"

SRAM.11
Associate III

Thank you I had find out solution for sleep mode and also found my AWU config wrong I am trying to correct that.Now my sleep mode have been executed but wakeup function not.It may be because of that halt function? when I am running my code in step by step debugger it says program went to halt .

Peter BENSCH
ST Employee

Have you configured the port pin as an input pin?
Have you set the interrupt on this port pin to the desired edge (falling, rising) and activated it?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SRAM.11
Associate III

Yes in stm8s003f  I couldn't find the EXTIPIN sensitivity but I set it for the port

Peter BENSCH
ST Employee

So far you haven't shown any code. How are the following registers configured:

  • CCR
  • PD_DDR
  • PD_CR1
  • PD_CR2
  • EXTI_CR1
  • PWR_CSR

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SRAM.11
Associate III
#include "stm8s.h"
#include "stm8s_clk.h"
#include "stm8s_adc1.h"
#include "stm8s_gpio.h"
#include "stm8s_tim2.h"
#include "main.h"
#include "flash.h"
//#include "stm8s_iwdg.h"
//#include "stm8s_awu.h"
#include "stm8s_exti.h"




volatile unsigned short _500ms_tick;
volatile unsigned short idle_counter;

void Clk_Config(void);
void ADC_Config(void);
void GPIO_Config(void);
void EXTI_Setup(void);
void ADC_Read1(uint16_t *MV);
void ADC_Read2(uint16_t *Vbat);
void ADC_Read3(uint16_t *Ocd);
void ADC_Read4(uint16_t *Temp) ;
	void AWU_Config(void);
main()
{
uint16_t MV=0,Vbat=0,Ocd=0,Temp=0;
	unsigned short i;
	int counting = 0;


	Clk_Config();
	
	ADC_Config();
	
	GPIO_Config(); 
		

	EXTI_Setup();

	
	while(MV<100)
	{
		ADC_Read1(&MV);
	 delay_ms(100);
		Set_LED(0);
		idle_counter++;
		
		if (idle_counter>=300)
		{
		
		 EnterSleepMode();
		}
    
	}
	
	              
	
	while (1)
	
	{
	ADC_Read1(&MV);
  delay_ms(100);
		
	ADC_Read2(&Vbat);
	delay_ms(100);
	
	ADC_Read3(&Ocd);
		delay_ms(100);
		
	ADC_Read4(&Temp);
  delay_ms(100);
	
    if (MV > 20) //                 Mains Detect
     //WakeupFromSleep();
		{
       if ((MV < 370) && (Vbat > 227))         // Mains Fail
					{
            En_Emergency(1); 
						Set_LED(0);
												
					}
			   			
        else 
        {
            En_Emergency(0);
						Set_LED(0);
			   }
				
			 
				
		}
		if(MV<=10)
		{
			ADC_Read3(&Ocd);
			delay_ms(100);
			Set_LED(0);
						if(Ocd<93 || Ocd>186)
						{
						Set_LED(1); 
						delay_ms(1000);	
						Set_LED(0); 
						delay_ms(1000);	
						Set_LED(1); 
						delay_ms(1000);	
						Set_LED(0); 
						delay_ms(1000);	
						Set_LED(1);
						delay_ms(1000);	
						Set_LED(0); 				
				
							delay_ms(5000);	
				
						}
				else if(Ocd>93 || Ocd<186)
				{
				Set_LED(0);
				}
			
	}
	
		ADC_Read2(&Vbat);
			if (MV < 250)
			{
				Set_LED(0);
			}
			else if(Vbat>460 || Vbat < 155)
			  {
					Set_Bch(1);
					Set_LED(0);
				}
			else if( Vbat>395)
			  {
					
					Set_LED(1); 
					Set_Bch(0);
				}
			else if(Vbat<383)
				{
						Set_LED(1); 
						Set_Bch(1);
				}
			ADC_Read4(&Temp);
			if(Temp>87 || Temp>425)
			{
				Set_Bch(1);
			}
			else //if(Vbat<87 || Vbat>425)
			{
			 Set_Bch(0);
				Set_LED(1); 
				delay_ms(1000);	
				Set_LED(0); 
				delay_ms(1000);	
				Set_LED(1); 
				delay_ms(1000);	
				Set_LED(0); 
				delay_ms(5000);
			 
			}
			
			

			
			


}
}



void Clk_Config()                          //  INTERNAL CLOCK CONFIGUARATION
	{
	CLK_DeInit();
	
	CLK_HSECmd(DISABLE);
	CLK_LSICmd(DISABLE);
	CLK_HSICmd(ENABLE);
	while(CLK_GetFlagStatus(CLK_FLAG_HSIRDY) == FALSE);
	
	CLK_ClockSwitchCmd(ENABLE);
	CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV2);
	CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);
	
	CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSI, 
	DISABLE, CLK_CURRENTCLOCKSTATE_ENABLE);
	

	CLK_PeripheralClockConfig(CLK_PERIPHERAL_ADC, ENABLE);
	 CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, ENABLE);
	}

void ADC_Config()                      //              ADC INITIALIZATION
	{
		 ADC1_DeInit();
		
		 ADC1_Cmd(ENABLE);

     ADC1_ITConfig(ADC1_IT_EOCIE, ENABLE);
		
	}
	
void ADC_Read1(uint16_t *MV)
{
	
	  ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS,     //   MAINS INPUT
					  ADC1_CHANNEL_5,
					  ADC1_PRESSEL_FCPU_D2, 
					  ADC1_EXTTRIG_GPIO, 
					  DISABLE, 
					  ADC1_ALIGN_RIGHT, 
					  ADC1_SCHMITTTRIG_CHANNEL5, 
					  DISABLE);
    ADC1_StartConversion();
    while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
    {
        // Wait for conversion to complete
    }

  *MV= ADC1_GetConversionValue();

}
void ADC_Read2(uint16_t *Vbat)
{
	  ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, //ADC Channel_4 VBATT
					  ADC1_CHANNEL_4,
					  ADC1_PRESSEL_FCPU_D2, 
					  ADC1_EXTTRIG_GPIO, 
					  DISABLE, 
					  ADC1_ALIGN_RIGHT, 
					  ADC1_SCHMITTTRIG_CHANNEL4, 
					  DISABLE);
    ADC1_StartConversion();
    while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
    {
        // Wait for conversion to complete
    }

  
	*Vbat=ADC1_GetConversionValue();
}
void ADC_Read3(uint16_t *Ocd)               // ADC Channel_2 OPEN CIRCUIT DETECTION
{
	  ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, 
					  ADC1_CHANNEL_2,
					  ADC1_PRESSEL_FCPU_D2, 
					  ADC1_EXTTRIG_GPIO, 
					  DISABLE, 
					  ADC1_ALIGN_RIGHT, 
					  ADC1_SCHMITTTRIG_CHANNEL2, 
					  DISABLE);
    ADC1_StartConversion();
    while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
    {
        // Wait for conversion to complete
    }

  
	*Ocd=ADC1_GetConversionValue();
}
void ADC_Read4(uint16_t *Temp)               // ADC Channel_2 TEMPARATURE MONITORING
{
	  ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, 
					  ADC1_CHANNEL_3,
					  ADC1_PRESSEL_FCPU_D2, 
					  ADC1_EXTTRIG_GPIO, 
					  DISABLE, 
					  ADC1_ALIGN_RIGHT, 
					  ADC1_SCHMITTTRIG_CHANNEL3, 
					  DISABLE);
    ADC1_StartConversion();
    while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
    {
        // Wait for conversion to complete
    }

  
	*Temp=ADC1_GetConversionValue();
}

void GPIO_Config(void)
	{
								//GPIO INPUTS
			
		//GPIO_Init(GPIOD,GPIO_PIN_2,GPIO_MODE_IN_FL_NO_IT);			// TEMP SENSE
		GPIO_Init(GPIOD,GPIO_PIN_3,GPIO_MODE_IN_FL_NO_IT);			//VBATT
		GPIO_Init(GPIOD,GPIO_PIN_5,GPIO_MODE_IN_FL_NO_IT);			//MAINS INPUT
		GPIO_Init(GPIOC,GPIO_PIN_4,GPIO_MODE_IN_FL_NO_IT);			// OCD SENSE
		
		
								//GPIO OUTPUTS
								
		GPIO_Init(GPIOA,GPIO_PIN_3,GPIO_MODE_OUT_PP_LOW_FAST);			// MAIN LAMP
		GPIO_Init(GPIOC,GPIO_PIN_3,GPIO_MODE_OUT_PP_HIGH_FAST);			//LED O/P
		GPIO_Init(GPIOC,GPIO_PIN_5,GPIO_MODE_OUT_PP_LOW_FAST);			//BCH
		
	}
void TIM2_Config(void)
{
    TIM2_TimeBaseInit(TIM2_PRESCALER_32768, 244);
    TIM2_ClearFlag(TIM2_FLAG_UPDATE);
    TIM2_ITConfig(TIM2_IT_UPDATE, ENABLE);
    TIM2_Cmd(ENABLE);
		AWU_DeInit();
		
		/* auto wake up at 32ms */
		AWU_Init(AWU_TIMEBASE_32MS);
		
		/* enable auto wake up*/
		AWU_Cmd(ENABLE);
		
		enableInterrupts();
}


  
INTERRUPT_HANDLER(TIM2_UPD_OVF_BRK_IRQHandler, 13)
{
    if (TIM2_GetITStatus(TIM2_IT_UPDATE) != RESET)
    {
			
        // Increment the idle_counter every 500ms
        idle_counter++;

        // Enter sleep mode if idle for approximately 30 seconds (60 * 500ms)
        if (idle_counter >= 300)
        {
            EnterSleepMode();
        }
				TIM2_ClearITPendingBit(TIM2_IT_UPDATE);
    }
}

void EnterSleepMode(void)
{
    // Disable TIM2 interrupt
    TIM2_ITConfig(TIM2_IT_UPDATE, DISABLE);

    // Disable ADC peripheral
    ADC1_Cmd(DISABLE);

    // Disable GPIO inputs
    GPIO_Init(GPIOD, GPIO_PIN_3, GPIO_MODE_IN_PU_NO_IT);
    GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_IN_FL_IT);
    GPIO_Init(GPIOC, GPIO_PIN_4, GPIO_MODE_IN_PU_NO_IT);

   halt();

    // Re-enable ADC peripheral
    
}

void Inc500mSCounter(void)
{
    if (_500ms_tick < 500)
    {
        _500ms_tick++;
    }
    else
    {
        _500ms_tick = 0;
        idle_counter++;
    }
}
/*void IWDG_Config(void)
	{
		uint8_t WTG_TIME;
	
		IWDG_Enable();
		
	
		IWDG_WriteAccessCmd(IWDG_WriteAccess_Enable);
		
		
		IWDG_SetPrescaler(IWDG_Prescaler_128);
		
		
		IWDG_SetReload( WTG_TIME);
		
		
		IWDG_ReloadCounter();
		
	}*/
/*void AWU_Config(void)
{
	AWU_Init(AWU_TIMEBASE_32MS);
		
	
		AWU_Cmd(ENABLE);
		
		enableInterrupts();
}*/




void EXTI_Setup(void)
{
	EXTI_DeInit();
	EXTI_SetExtIntSensitivity(EXTI_PORT_GPIOD, EXTI_SENSITIVITY_RISE_ONLY);
	EXTI_SetTLISensitivity(EXTI_TLISENSITIVITY_RISE_ONLY);

}

void WakeupFromSleep(void)
{
	ADC1_Cmd(ENABLE);

    // Re-enable GPIO inputs
    GPIO_Init(GPIOD, GPIO_PIN_3, GPIO_MODE_IN_FL_NO_IT);
    GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_IN_FL_NO_IT);
    GPIO_Init(GPIOC, GPIO_PIN_4, GPIO_MODE_IN_FL_NO_IT);

    // Reset idle counter
    idle_counter = 0;

    // Re-enable TIM2 interrupt
    TIM2_ITConfig(TIM2_IT_UPDATE, ENABLE);
    
}
INTERRUPT_HANDLER(EXTI_PORTD_IRQHandler, 6)
{
	 //EXTI_ClearITPendingBit(EXTI_PORT_GPIOD);
    {        // Wake up from sleep mode
        WakeupFromSleep();
    }
}



for this code my sleep function is working if i enable Apologies for any confusion in this code as I am literally working on it to sort it out .I am in an independent work environment no teams to help it out.Little struggle in developing the code