cancel
Showing results for 
Search instead for 
Did you mean: 

USING CELLING FAN REMOTE CONTROL UNIT BASED ON THE STM8 MICROCONTROLLER.

VRAMA.11
Associate

 I am Searching on your site STEVAL-IHM037V1, IR Transmitter and receiver BOARD and circuit, also i have a transmitter code using chip STM8L101F2P66.

BUT i don"t have the code of receiver using IC STM8S003F3P6, I have to develop some kind of R&D product using same chip transmitter and receiver . so can u provide me the code (firmware) of receiver so that i can use your chip.

Please provide a me a proper solution as much as u can.Because i need 1000 's of pcs (min)

thanks

4 REPLIES 4
Ozone
Lead III

You better approach a ST sales person, FAE, or distributor directly.

This is a user support forum, mostly discussing technical issues amongst users (and a few technical ST staff).

When source isn't immediately downloadable it usually means you need to license directly from ST, or gain access via your local sales office. Substantial engineering support would likely need 100K units, a history of, rather than potential for.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
VVamv.1
Associate

Can you please share the transmitter code for the STEVAL-IHM037V1

The product is obsolete.

Materials related to it would need to be requested via a local sales office or representative.

Apt to be licencing or liability waivers involved.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..