2020-04-23 5:34 AM
Hello,
I'm trying to implement serial communication between a stm8al3l68 an a serial terminal installed on my PC.
The problem is that there is no virtual port on my STM8 as on STM32.
How can I communicate with the PC if there is no virtual Port. What kind of hardware should i buy ?
--> HCCABL0015 USB to RS232 TTL Serial Interface Cable like explained there : http://www.colecovision.eu/stm8/STM8S-DISCOVERY%20Serial.shtml
And when I'll have this hardware, i just have to init USART with :
STM_EVAL_COMInit(COM1, (uint32_t)115200, USART_WordLength_8b, USART_StopBits_1,
USART_Parity_No, (USART_Mode_TypeDef)(USART_Mode_Tx | USART_Mode_Rx));
USART_Cmd(EVAL_COM1, ENABLE);
and send data with
void USART_SendData8(USART_TypeDef* USARTx, uint8_t Data)
Another question, how can I know if I have to include stm8l1526_eval.h or stm8l1528_eval.h header files ?
I'm really lost with STM8 MCU, need some help ! Thank you all !
Best Regards,
AJT
2020-04-23 11:40 AM
"How can I communicate with the PC if there is no virtual Port" - The STM8 has a real hardware USART port, much like an STM32. If you want to use it to communicate with a PC, you will need on the PC side another USART port, with same voltage levels (3.3V). If you don't have it, you will need a converter in between.
In case you use an ST development board, it might already have all you need, through a USB interface.
My advice: don't try to do all in 30 min with 20 mouse clicks! Take the time to understand what you work with, and surely this time will be rewarded.
2020-04-23 1:08 PM
Hello Cristian, thanks for you answer !
First of all i'm going to check is something is sent via STM8AF_USART_TX with an oscilloscope.
Then i'll try to use this (because i found one) : https://www.st.com/en/development-tools/stlink-v3set.html
Sounds like i can create a virtual com port with that but I don't really know to what should I connect STM8AF_USART_TX and STM8AF_USART_RX. Well, to my mind i must connect STM8AF_USART_TX to stlink-v3 RX and STM8AF_USART_RX to stlink-v3 TX.
Here are some screenshots to explain why i should do that :
Screenshot of stlink-v3 datasheet that talks about VCP
Screen shot of STM8AL3L68 datasheet
and finally a screen of the hardware board MB1440 that is included in stlink-v3
Tell me if I'm wrong !
Best Regards,
AJT
2020-04-30 10:47 AM
Ok i found the solution, the problem came from SB4 and SB5 that there were not Fitted