cancel
Showing results for 
Search instead for 
Did you mean: 

Unique ID Returning Zeros

davidbleakley9
Associate II
Posted on September 29, 2011 at 12:41

I am using ST Visual Develop

STM8S105xx Datasheet Page 57 details the 96-bit unique device identifier

My Device is STM8S105K6

I am using stm8s_flash.c to call the FLASH_ReadByte function as follows:

for (i=0; i<12; i++)

            u_id[i] = FLASH_ReadByte(0x48CD+i);

u_id is filled with zeros.

I looked in the memory view and this location also appears to be filled with zeros.

I can read other locations as expected.

The Flash Registers are:

[0x505a] FLASH_CR1 - Flash control register 1

0x00

[0x505b] FLASH_CR2 - Flash control register 2

0x00

[0x505c] FLASH_NCR2 - Flash complementary control register 2

Intrusive read

[0x505d] FLASH_FPR - Flash protection register

0x00

[0x505e] FLASH_NFPR - Flash complementary protection register

0xff

[0x505f] FLASH_IAPSR - Flash in-application programming status register

Intrusive read

[0x5062] FLASH_PUKR - Flash Program memory unprotection register

0xae

[0x5064] FLASH_DUKR - Data EEPROM unprotection register

0x56

The option Bytes are

AFR1

Default

AFR2

Alternate Ative

AFR3

Default

AFR4

Default

AFR5

Default

AFR6

Default

AFR7

Default

CKAWUSEL

Low Speed Internal

EXTCLK

External Oscillator

HSECNT0

0

HSECNT1

0

HSECNT2

0

HSECNT3

0

HSECNT4

0

HSECNT5

0

HSECNT6

0

HSECNT7

0

HSITRIM

3-bit trimming

IWDG HW

Software

 LSI_EN

 Disabled

PRSC

16MHz to 128kHz

ROP

Read-out protection disabled

UBC

Write protection disabled

WWDG_HALT

No Reset

WWDG_HW

Software

l2C

Frozen when stopped

Timer1

Frozen when stopped

T�mer2

Frozen when stopped

T�mer3

Frozen when stopped

T�mer4

Frozen when stopped

A combination of the following may be true:

  1. I have not set up something correctly.
  2. I have managed to erase this location.
  3. I have got a dodgy device.
Any Ideas?

#stm8-stm8s105-unique-id-96-bit
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
davidbleakley9
Associate II
Posted on November 09, 2011 at 18:54

I have received the following from ST:

The unique ID's are being programmed inside the STM8 products during their production only from second half of 2010. If you get samples with marking ending by for example MYS 11xx, those should be OK. 11 stands for the year, xx for the week.