Timer synchronicity between channels
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-11-27 2:42 AM
Posted on November 27, 2013 at 11:42
Hello,
I am using a STM8L151K6T3 and need for synchronous rectifier purposes two clock signals with the same frequency, which both have to be absolutely of a symmetric rectangle shape. Secondly I do need a possibility to adjust the phase between these two clocks. Thus I decided to use Timer1 with two channel outputs and toggle mode. For initializing there are two lines: (1) TIM1-> CCMR1 = 0b00111000; //Preload enable, OCM = 011 (Toggle), CC1S output TIM1-> CCMR2 = 0b00111000; //Preload enable, OCM = 011 (Toggle), CC2S output The phase adjusting is done by these: (2) TIM1-> CCR2H = 0; TIM1-> CCR2L = Par_SG_Phase; If I omit the lines of (1), then it happens sometimes that both clocks could jump in phase of 180°(thus one clock is inverted) when a phase adjust event is there. Of course this is unwanted. But is it guaranteed that with (1) the phase relationship is frozen forever? Or can it happen again by an interference or so? I think, because in toggle mode we have two independent flipflops driven by Timer1, the states of the flipflops are defined at the very beginning after initializing only. Or what does the Preload enable exactly? The reference manual for the STM8 is not clear for me at the place where CCMR register is described. I have to add, that I never ever had noticed any event of the above described phase inversion, since (1) was added into my code. Everything else is working fine, but I still worry about this, because an occur could have fatal results. Best regards Dieter
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-06-24 9:01 PM
Posted on June 25, 2014 at 06:01
i am generating pulse of 10us for on and 8 us for off in TIM1_CH3 and TIM1_CH4 i want to 1us delay between these two signal............how is it possible plz help me if any one know about this ...thanks