cancel
Showing results for 
Search instead for 
Did you mean: 

Timer 1 CC and Timer 2 as PWM

daschenbrenner
Associate II
Posted on January 27, 2015 at 13:27

Hi all,

is it possible to run the Timer 1 in Capture Compare mode to detect the duty cycle of a PWM and the Timer 2 in Capture Compare mode to generate a PWM?

Sadly in my project Timer 2 is not giving any output while i measure the duty cycle with Timer 1.

CODE:

/* Configure TIMER1 peripheral -----------------------------------------------*/

static void TIM1_Config(void)

{

/* Init TIMER 1 */

  CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER1, ENABLE);

  // configure TIM1 channel 1 to capture a PWM signal

  TIM1_PWMIConfig(TIM1_CHANNEL_1, TIM1_ICPOLARITY_RISING, TIM1_ICSELECTION_DIRECTTI,

                  TIM1_ICPSC_DIV1, ENABLE);

  // Select the TIM1 Input Trigger: TI1FP1

  TIM1_SelectInputTrigger(TIM1_TS_TI1FP1);

  TIM1_SelectSlaveMode(TIM1_SLAVEMODE_RESET);

  // Enable CC1 interrupt request

  TIM1_ITConfig(TIM1_IT_CC2, 0x01);

  // Enable TIM1

  TIM1_Cmd(ENABLE);

  enableInterrupts();

} static void TIM2_Config(uint16_t value)

{

 //CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, ENABLE);

  TIM2_TimeBaseInit(TIM2_PRESCALER_1, 16000);                 // Time base configuration

  TIM2_OC1Init(TIM2_OCMODE_PWM1, TIM2_OUTPUTSTATE_ENABLE,value, TIM2_OCPOLARITY_HIGH);

  TIM2_OC1PreloadConfig(ENABLE);                       // PWM1 Mode configuration: Channel1

  TIM2_ARRPreloadConfig(ENABLE);

  TIM2_Cmd(ENABLE);                              // TIM2 enable counter

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0