2010-05-12 2:35 AM
STVD error while opening workspace
2011-05-17 6:08 AM
.ExternalClass716313A724AC41C5B5BF97C72915FDEB p.MsoNormal, .ExternalClass716313A724AC41C5B5BF97C72915FDEB li.MsoNormal, .ExternalClass716313A724AC41C5B5BF97C72915FDEB div.MsoNormal {margin-top:0in;margin-right:0in;margin-bottom:10.0pt;margin-left:0in;line-height:115%;font-size:11.0pt;font-family:'Calibri','sans-serif';} .ExternalClass716313A724AC41C5B5BF97C72915FDEB .MsoChpDefault {;} .ExternalClass716313A724AC41C5B5BF97C72915FDEB .MsoPapDefault {margin-bottom:10.0pt;line-height:115%;} @page Section1 {size:595.35pt 841.95pt;margin:1.0in 1.0in 1.0in 1.0in;} .ExternalClass716313A724AC41C5B5BF97C72915FDEB div.Section1 {page:Section1;}
Hi Remi,
Your default configuration for the stvd project are updated, so to avoid this issue use a personalized path when create a new project You can resolve this issue by updating your local files dafault.wed and default.wdb available under ''$:\Program Files\STMicroelectronics\st_toolset\stvd'' with attached Regards mozra2011-05-17 6:08 AM
Hi Mozra
This does not really fix the problem
The sharing violation occurs and the workspace files get corrupted again...
The only solution I have is change the workspace files each time it occur (really annoying)
Thx anyway
2011-05-17 6:08 AM
I'm seeing a very similar corruption in my project/workspace files. It seems that each time I open my workspace (.stw file), it's adding a bunch of data to the .wed file.
I tried to attach by before and after .wed file, but the forum wouldn't let me. I kept getting a ''The file or folder name contains characters that are not permitted'' error.
If you want to see them let me know what email address I can send them. -s2011-05-17 6:08 AM
Actually, replacing the default wdb and wed files seems to have resolved it for me.
Should have tried that first, thanks!
-s
2011-05-17 6:08 AM
The solution seems to be short-lived. I still get corruption commonly, and have to restore the default files again. Why are the default files being modified by opening my workspaces?
spencer