cancel
Showing results for 
Search instead for 
Did you mean: 

stm8s207mb controller working only in debug

kishor
Associate II

 Hi Sir ,

   This is kishor ,we are using stm8s207mb in our application, some board are working in debug mode only , when we come out from debug its not running . iam not able to understand the  problem . is there any ide issue or hard ware issue . we noticed one point in working  board Reset Pin maintaining 3.5v, in the problem board  it is below 2.6v . but we are  using same components  in all boards ....

 please help me these problem Thank you.......

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome @kishor, to the community!

There are a myriad of possible scenarios why the STM8 won't work for you without a debugger connected. Without more details on the environmental conditions (schematics, parameters, etc), probably nobody is able to help you.

For example, pin NRST on the STM8S207 is a bidirectional pin, as you can see from RM0016, section 8. You should therefore look at this pin with an oscilloscope and not just measure a DC voltage with a multimeter.

Furthermore, for proper work, cleanly created software is necessary - it is certainly not exactly the same as in the other, working boards, is it?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.