cancel
Showing results for 
Search instead for 
Did you mean: 

STM8S105 2 channel ADC1 problem

idurgun
Associate
Posted on November 20, 2014 at 11:41

Hi All

I want to read 2 channel ADC from ADC1 library. You can see my code below. I used scan mode and conversation mode single. I take 4 samples in interrupt and used average of them in my main code. My problem is sometimes ADC1_GetBufferValue(1) or ADC1_GetBufferValue(0) returns bigger than 1023. For example 20000, 40000 or something like that. Could you have any opinion for this issue ?

void ADC_Configuration(void)

{

ADC1_DeInit();

ADC1_Cmd(ENABLE);

ADC1_Init(ADC1_CONVERSIONMODE_SINGLE, ADC1_CHANNEL_1, ADC1_PRESSEL_FCPU_D18, \

ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_ALL, DISABLE);

ADC1_ScanModeCmd(ENABLE); 

ADC1_ITConfig(ADC1_IT_EOCIE, ENABLE);

ADC1_DataBufferCmd(ENABLE);

ADC1_StartConversion();

}

 INTERRUPT_HANDLER(ADC1_IRQHandler, 22)

 {

ADC1_ClearITPendingBit(ADC1_IT_EOC);

//ADC1_ClearFlag(ADC1_FLAG_EOC); 

wBATTERY_VOLTAGE_SUM = wBATTERY_VOLTAGE_SUM + ADC1_GetBufferValue(1);

byBATTERY_VOLTAGE_SAMPLE_COUNT++;

if(byBATTERY_VOLTAGE_SAMPLE_COUNT > 3)

{

wBATTERY_VOLTAGE = wBATTERY_VOLTAGE_SUM>>2;

wBATTERY_VOLTAGE_SUM = 0;

byBATTERY_VOLTAGE_SAMPLE_COUNT = 0;

}

wBOOST_VOLTAGE_SUM = wBOOST_VOLTAGE_SUM + ADC1_GetConversionValue();

byBOOST_VOLTAGE_SAMPLE_COUNT++;

if(byBOOST_VOLTAGE_SAMPLE_COUNT > 3)

{

wBOOST_VOLTAGE = wBOOST_VOLTAGE_SUM>>2;

wBOOST_VOLTAGE_SUM = 0;

byBOOST_VOLTAGE_SAMPLE_COUNT = 0;

}

 }

#adc1 #stm8s
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0