STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Program four STM8 in parallel.

Posted on December 09, 2013 at 19:15Hi,This is my first post so hi everyone. I would like to program the four STM8 in parallel.I would like to use for this ''STVP_CmdLine.exe'' and ST-Link's V2.  I know that the programmers have different numbers VI...

s_michas by Associate
  • 624 Views
  • 1 replies
  • 0 kudos

STM8 Programmer tool

Posted on May 17, 2013 at 06:53Hi All, am developing one programmer tool as like ST visual tool , for flashing s19 file.but i dont have API for that . but in website mentioned use PtkApi.cpp but this cant able to download , if any one have idea abou...

rajeeva by Associate
  • 656 Views
  • 1 replies
  • 0 kudos

Urgent: STM8S003F3 reset pin gets damaged

Posted on December 05, 2014 at 14:58I am using STM8S003F3 & attached is circuit. I have connected some switches in pull-up configuration as shown. After some correct operations, I have seen that some of boards stopped working. It was problem 1 as ...

STM8L Interrupt

Posted on October 29, 2014 at 17:07Hello, I'm using the STM8L151 using IAR workbench without ST Firmware Library and I'm trying to use an SPI Interrupt. Unfortunatey it doesn't work. SPI is already running, the receiving flag is set, but i don't get...

STM8 Evaluation- Independent watchdog

Posted on December 01, 2014 at 08:15Hello,  According to reference manual IWDG will not be stopped even after entering HALT mode. Is there a possibility to STOP or PAUSE IWDG for STM8A ? According to STM8AL we can halt IWDG, but STM8AL is not suitab...

kawasthi by Associate
  • 572 Views
  • 0 replies
  • 0 kudos

Active halt low power mode

Posted on November 11, 2013 at 12:34HiWe are developing with STM8L152C6 microcontroller and debugging using the discovery board.Our application uses a battery when there is no power. In this case, we need only two I/O interrupts and the LCD to be wo...

design by Associate
  • 1459 Views
  • 3 replies
  • 0 kudos

STM8S105 2 channel ADC1 problem

Posted on November 20, 2014 at 11:41Hi AllI want to read 2 channel ADC from ADC1 library. You can see my code below. I used scan mode and conversation mode single. I take 4 samples in interrupt and used average of them in my main code. My problem is...

idurgun by Associate
  • 707 Views
  • 0 replies
  • 0 kudos

I have STM8S Discovery examples, Fuzzy Logic, Power System Relay

Posted on April 26, 2011 at 06:32Hello All, I used to teach at a university in Ontario; I switched to another job in the industry. I have developed a number of simple examples meant to gradually introduce students to programming the STM8S Discovery ...

STM8 SWIM pin as output/Debug

Posted on November 08, 2014 at 11:361. I have STM8S003F3 & want to use its debug pin as output. So I will configure it my code.2. Will that make debug option dead?On next power up, will I be able to debug the code?? Because pin will already be confi...

[HELP] The diffrence of Option Bytes between IAR and STVP

Posted on November 08, 2014 at 09:50I have just began with STM8 and I use IAR. I'm in trouble with Option Bytes with both of IAR and STVP. They have some differences between them. I use STM8S105C6T6 chip. I also searched in datasheet, user manual, r...