2017-01-18 11:59 AM
Hi,
i use IAR EWSTM8 to debug and flash the STM8S103F3 controller which i have here on a small blue breakout board. Yesterday i flashed the Controller via the ST-Link V2 as always but instead of going into the debug menu, IAR gave me this on the console:
C-SPY Processor Descriptor V2.20.1.176 for STM8
C-SPY Debugger Driver, ST-LINK V2.20.1.176 for STM8 Failed to set configuration with MCU name STM8S103F3P: SWIM error [30006]: Comm init error: chip does not answerThe last code i successfully uploaded was this:
#include ''iostm8s103f3.h''
#pragma vector = TIM4_OVR_UIF_vector
__interrupt void TIM4_UPD_OVF_IRQHandler(void){ PC_ODR ^= (1<<4); //Toggle Pin TIM4_SR &=~(1<<0); //Clear Update interrupt flag}void initTimer(){
CLK_PCKENR1 |= (1<<4); //Enable Clock for Timer 4 TIM4_PSCR = (0x0F); //Prescaler, Divide Clock by Max TIM4_IER = 1; //Enable Update Interrupt TIM4_CR1 |= 1; //Enable Timer asm(''rim''); //Enable Interrupts }void initGPIO(){
PC_DDR |= (1<<4); //Set Pin as Output PC_CR1 |= (1<<4); //Set Pin as PushPull PC_ODR |= (1<<4); //Set to High}void main()
{ initTimer(); initGPIO(); CLK_CKDIVR = 0x08; while(1){ ; }}I was told to pull the NRST-Pin of the board to GND while switching power on / off and then try again, but that didn't help. I also tried to flash via STVP but i got this error message:
The last program i flashed works fine but putting a new program on the chip doesn't work
:(
Anyone here who has a solution / ideas to this problem?Best regards2017-01-22 04:49 AM
maybe your NRST pin was Pulled down by hardware
i have same problem in the past
or you have high Impedance
junction between VCC and GND
2017-01-22 06:06 AM
Hi and thanks alot for your answer,
maybe your NRST pin was Pulled down by hardware
What do you mean? Why should the board pull the NRST pin to GND from one moment to another? As i said i pulled the NRST pin to low (via a jumper wire) to mimic the SWIM-Initialization.
Could you explain in detail how you fixed the problem in the past, please?Best regards2017-01-22 08:50 AM
in my case the reset button was burn
so my MCU was reset Continuously
but in your case i dont know so much
i suggest you that put an amper meter before your supply and Measure the board amper
so you find that any part of you PCB is burn or not
Excuse me for my English
2017-02-21 11:31 PM
Hi all, I have a similar problem with ST-Link V2 and IAR, but there are some diffirent things in my case. To be more specific, I use 4 wire of ST-link: RST, SWIM, GND and 5V for first case, 3.3V for second case.
In first case, when I use 5VDC line, I can load code and debug successfully, and everything is fine.
But, in second case, when I use 3.3VDC line to load code, IAR display the message '
Failed to set configuration with MCU name STM8S105C6: SWIM error [30006]: Comm init error: chip does not answer
'. And, if I use 5V to load code then I use 3.3V to supply power, STM8S105C6 still not work.It seems that STM8S105C6 cannot operate at 3.3V, while datasheet show that it can work from 2.95V to 5.5V.
Anyone here who has ideas to this problem?
(
Excuse me for my English
)Best regards