cancel
Showing results for 
Search instead for 
Did you mean: 

uint8_t TI_TDC1000_SPIByteReadReg(uint8_t addr) { uint8_t read_byte,inst; uint8_t dummy = 0x00; inst = TDC1000_READ_BIT

np1
Associate II
Posted on February 21, 2017 at 09:33

Dear all,

here is my code to read spi data:

uint8_t TI_TDC1000_SPIByteReadReg(uint8_t addr)

{

uint8_t read_byte,inst;

uint8_t dummy = 0x00;

inst = TDC1000_READ_BIT & addr; // for read make sure bit6 is 0

//GPIO_ResetBits(TI_TDC1000_CSn_PORT ,TI_TDC1000_CSn_PIN); // CS enable

while (SPI_GetFlagStatus(SPI1, SPI_FLAG_TXE)== RESET);

SPI_SendData(SPI1, inst);

while (SPI_GetFlagStatus(SPI1, SPI_FLAG_TXE)== RESET);

SPI_SendData(SPI1, dummy);

/* Wait to receive a byte */

while (SPI_GetFlagStatus(SPI1, SPI_FLAG_RXNE) == RESET);

/* Return the byte read from the SPI bus */

read_byte = SPI_ReceiveData(SPI1);

return read_byte;

}

I using oscilloscope and see that the data is read = 0x45, but in my code 

read_byte alway = 0xFF, I think somewhere wrong when spi recieve data.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
S.Ma
Principal
Posted on February 21, 2017 at 11:51

Change the wait events for waiting for RXNE.

When TXE is set, the SPI is just starting to spit the byte out (and a new one can be pre-loaded)

When RXNE is set the whole byte has been shipped and one has arrived for reading.

You can toggle a GPIO to view when each wait happens respective to the SPI Clocks to debug.

np1
Associate II
Posted on February 22, 2017 at 04:00

Hi,

I toogle GPIO and see SPI_FLAG_RXNE = SET after recieved all data, I think that is correct?

Could you suggest me what i must fix with this bug?

'

Change the wait events for waiting for RXNE.

'  what should I change?

Thanks

Posted on February 22, 2017 at 09:26

Try replacing all the TXE flag test by RXNE flag test and see what happens.

Posted on February 22, 2017 at 09:27

wait for RXNE = 1