STM8S UART Receive problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-02 4:24 AM
I have a weird condition in which the STM8S003 does not read the entire packet I'm sending using a PC serial port. For example I have sent 256 bytes using a PC software but at the end I have only read 214 bytes instead of 256 bytes in the controller. (RX ISR happened 214 times instead of 256 times)
What could be possibly wrong? It's said a read to the Data Register is enough to clear the flags.I'm going crazy here because it's not supposed to be this hard getting a simple RX interrupt to work. #stm8s-uart- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-11-17 8:43 AM
I wonder if you were able to solve this problem? I'm currently having the same issue with a stm8s207
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-10 7:39 AM
HI!
I do it!
//////////////////////////////////////////////////////////////////////////////////////
#include "stm8s.h"
#include "stm8s_uart1.h"
#include "stm8s_clk.h"
uint8_t RxBuffer1[5];
__IO uint8_t RxCounter1 = 0x00;
static void UART_Config(void);
void main(void)
{
/* CLK configuration -----------------------------------------*/
CLK_Config();
static void UART_Config(void)
{
// Deinitializes the UART1 peripheral //
UART1_DeInit();
/* UART1 configuration -------------------------------------------------*/
/* UART1 configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Receive and transmit enabled
- UART1 Clock disabled
*/
/* Configure the UART1 */
UART1_Init((uint32_t)9600, UART1_WORDLENGTH_8D, UART1_STOPBITS_1, UART1_PARITY_NO,
UART1_SYNCMODE_CLOCK_DISABLE, UART1_MODE_RX_ENABLE);
/* Enable UART1 Transmit interrupt*/
// UART1_ITConfig(UART1_IT_TXE, ENABLE);
/* Enable UART1 Receive interrupt */
UART1_ITConfig(UART1_IT_RXNE_OR, ENABLE);
/* Enable general interrupts */
enableInterrupts();
}
INTERRUPT_HANDLER(UART1_RX_IRQHandler, 18)
{
/* Read one byte from the receive data register */
uint8_t dados[1] = {0x00};
dados[0] = UART1_ReceiveData8();
if(RxCounter1 <= 3)
{
RxBuffer1[RxCounter1] = dados[0];
IncrementVar_RxCounter1();
}
else
{
RxBuffer1[RxCounter1] = dados[0];
RxCounter1 = 0;
}
uint8_t GetVar_RxCounter1(void)
{
return RxCounter1;
}
uint8_t IncrementVar_RxCounter1(void)
{
return RxCounter1++;
}
static void CLK_Config(void)
{
/* Initialization of the clock */
/* Clock divider to HSI/1 */
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
}