2012-01-20 6:43 AM
Hi i have problem about Usart interrupt . I checked everything i use RFI interface for transmit and receive data. I can transmit data correctly(i checked with USBee) but my mcu not calculate receive data. Problem can be about configuration options but i'm not sure. Can anybody help me about this subject?
exam :
if(USART_DataInRxBuffer()) { if(USART_Rx()==0x50) { GPIO_SetBits(LEDS_PORT,LED1); //Everything right about GPIO Options I didn't write here Delay((uint32_t)60000); GPIO_ResetBits(LEDS_PORT,LED1); Delay((uint32_t)10000); } } /////////////////////////// DEFINES///////////////////////////////&sharpdefine USART_RX_BUFFER_SIZE 128 /* 2,4,8,16,32,64,128 or 256 bytes */&sharpdefine USART_TX_BUFFER_SIZE 128 /* 2,4,8,16,32,64,128 or 256 bytes */&sharpdefine USART_RX_BUFFER_MASK ( USART_RX_BUFFER_SIZE - 1 )&sharpdefine USART_TX_BUFFER_MASK ( USART_TX_BUFFER_SIZE - 1 )&sharpif ( USART_RX_BUFFER_SIZE & USART_RX_BUFFER_MASK ) &sharperror RX buffer size is not a power of 2&sharpendif&sharpif ( USART_TX_BUFFER_SIZE & USART_TX_BUFFER_MASK ) &sharperror TX buffer size is not a power of 2&sharpendif // Rx Buffertypedef unsigned char uint8_t ;static unsigned char USART_RxBuf[USART_RX_BUFFER_SIZE];static volatile unsigned char USART_RxHead;static volatile uint8_t USART_RxTail;static volatile uint8_t USART_RxOverflow;// Tx Buffer/static unsigned char USART_TxBuf[USART_TX_BUFFER_SIZE];static volatile uint8_t USART_TxHead;static volatile uint8_t USART_TxTail;void Delay(uint32_t nCount);void USART_RX_IRQHandler(void);void USART_TX_IRQHandler(void);unsigned char USART_Rx( void );uint8_t USART_DataInRxBuffer( void );/////////////////////////////// USART OPTIONS ///////////////////////////////////enableInterrupts(); CLK_MasterPrescalerConfig(CLK_MasterPrescaler_HSIDiv1);//High speed internal clock prescaler: 1GPIO_ExternalPullUpConfig(GPIOC,GPIO_Pin_2|GPIO_Pin_3, ENABLE);//Set the USART RX and USART TX at high level//<---IS THAT TRUE ????///////////////
CLK_PeripheralClockConfig(CLK_Peripheral_USART, ENABLE);// Enable USART clock USART_DeInit();USART_Init((uint32_t)9600, USART_WordLength_8D, USART_StopBits_1, USART_Parity_No, USART_Mode_Rx|USART_Mode_Tx);// Enable the USART Transmit interrupt: this interrupt is generated when the USART transmit data register is empty //USART_ITConfig(USART_IT_TXE, ENABLE);// Enable the USART Receive interrupt: this interrupt is generated when the USART receive data register is not empty USART_ITConfig(USART_IT_RXNE, ENABLE);USART_Cmd(ENABLE)////////////////////////////////////////////BUFFER FUNCTIONS//////////////////////////////////void USART_RX_IRQHandler(void) { unsigned char RxData; uint8_t tmphead; /* Read one byte from the receive data register */ RxData = (uint8_t) (USART_ReceiveData8() & 0x7F); //Read the received data tmphead = (USART_RxHead + 1) & USART_RX_BUFFER_MASK; //Calculate buffer index USART_RxHead = tmphead; // Store new index if (tmphead == USART_RxTail) { /* ERROR! Receive buffer overflow */ /* data will get lost !!! */ USART_RxOverflow = 1; } else { USART_RxBuf[tmphead] = RxData; // Store received data in buffer USART_RxOverflow = 0; }}uint8_t USART_DataInRxBuffer( void ){ return ( USART_RxHead != USART_RxTail); /* Return 0 (FALSE) if the receive buffer is empty */}unsigned char USART_Rx( void ){ uint8_t tmptail; //see if we have any data while ( USART_RxHead == USART_RxTail ); tmptail = (USART_RxTail + 1) & USART_RX_BUFFER_MASK; USART_RxTail = tmptail; return USART_RxBuf[tmptail]; } void Delay(uint32_t nCount){ /* Decrement nCount value */ while (nCount != 0) { nCount--; }} #stm8l101xx #usart #buffer2012-02-16 4:24 AM
a couple of things I have noticed about your code
head and tail are not initialised. Also you appear to be adding new received chars to the head of the Q and removing from the tail. Surely you should add to the tail ( latest char ) and remove form the head (oldest char) for FIFO.