cancel
Showing results for 
Search instead for 
Did you mean: 

stm8 stvd error in build

memet tri cahyono
Associate
Posted on October 06, 2017 at 18:02

dear all, i'm ner in stm8 MCU. i use stvd to coding, and it was okey to compile. but when i try to build i got error

Compiling main.c...

cxstm8 +mods0 +debug -pxp -no -l -i..\..\downloads\stm\stm8 -i..\..\downloads\stm\stm8\spl\en.stsw-stm8069\stm8s_stdperiph_lib\libraries\stm8s_stdperiph_driver\inc -i'C:\Program Files\COSMIC\CXSTM8_EVAL\Hstm8' -clDebug\ -coDebug\ main.c

main.c:

Running Linker

clnk -m Debug\spl.map -l'C:\Program Files\COSMIC\CXSTM8_EVAL\Lib' -o Debug\spl.sm8 Debug\spl.lkf

#error clnk Debug\spl.lkf:1 symbol _assert_param not defined (Debug\stm8s_gpio.o )

The command: 'clnk -m Debug\spl.map -l'C:\Program Files\COSMIC\CXSTM8_EVAL\Lib' -o Debug\spl.sm8 Debug\spl.lkf ' has failed, the returned value is: 1

exit code=1.

spl.elf - 3 error(s), 0 warning(s)

does anyone can help? thanks......

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Pavel A.
Super User
Posted on October 15, 2017 at 01:23

Somewhere in the project you have defined macro USE_FULL_ASSERT

Remove it.

If you don't want to remove this macro or don't know where it is defined, then add the following function in one of your source files:

void assert_param(uint8_t* file, uint32_t line)

{

     /* User can add his own implementation to report the file name and line number,

     ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */

}

Regards,

-- pa