cancel
Showing results for 
Search instead for 
Did you mean: 

STM8 internal temperature sensor

jakub23
Associate
Posted on September 06, 2016 at 10:20

I am working on a project, which is based on STM8 MCU.

I am using ADC to read the ambient temperature. Sometimes I am getting temperature ADC readings which are greater than the usual ones. Most of the time the samples are 608-611, and sometimes they reach value as high as 620 (in the same ambient temperature).

I reproduced this in a simple program, which has the following loop:

Init;

configure RTC to wakeup every 100ms;

initialize ADC;

enable interrupts;

while (1) {

  rtc wakeup enable;

  halt;

  rtc wakeup disable;

  read ADC temperature value;

}

I have the following ADC configuration for reading temperature:

ADC_Init(ADC1, ADC_ConversionMode_Continuous, ADC_Resolution_12Bit, ADC_Prescaler_2);

ADC_SamplingTimeConfig(ADC1, ADC_Group_FastChannels, ADC_SamplingTime_96Cycles);

STM8 clock external is 12MHz, VDD=3.3V.

What could the reason of such differing values?

#stm8
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John7
Associate II
Posted on November 24, 2016 at 18:05

Hi,

Just guessing as you did not provide info about the temperature sensor hardware.

Possible causes for deviating ADC values:

 - Ripple / disturbance / noise / hum on ADC reference voltage if external.

 - Ripple / disturbance / noise / hum on MPU Vdd if ref. voltage internal.

 - Ripple / disturbance / noise / hum on temperature sensor signal.

 - Current Injection into other ADC-channels.

HTH,

John7