cancel
Showing results for 
Search instead for 
Did you mean: 

PWM input capture

gibba
Associate II
Posted on December 18, 2013 at 17:59

Hi,

I'm trying to read a 5kHz square wave dc=50%. I'm using thw pwm input capture.

The problem is that the program gives me a dc=100% and strange frequencies, but i cannot figure out why it happens.. can someone help me? 

 /******************main****************/

/* Init TIMER 1 */

  CLK_PeripheralClockConfig(CLK_Peripheral_TIM1, ENABLE);

  // configure TIM1 channel 1 to capture a PWM signal

  TIM1_PWMIConfig(TIM1_Channel_2, TIM1_ICPolarity_Rising, TIM1_ICSelection_DirectTI,

                  TIM1_ICPSC_DIV1, TIM1_ICFilter);

  // Select the TIM1 Input Trigger: TI1FP1

  TIM1_SelectInputTrigger(TIM1_TRGSelection_TI1FP1);

  TIM1_SelectSlaveMode(TIM1_SlaveMode_Reset);

  // Enable CC1 interrupt request

  TIM1_ITConfig(TIM1_IT_CC2, ENABLE);

  // Enable TIM1

  TIM1_Cmd(ENABLE); 

  

  enableInterrupts();

/**********interrupt

INTERRUPT_HANDLER(TIM1_CAP_IRQHandler, 24)

{

disableInterrupts();

  /* Get the Input Capture value by reading CCR1 register */

  /* CCR1 regsiter contains signal frequency value */

  IC1Value = TIM1_GetCapture2();

  if (IC1Value != 0)

  {

    /* Get the Input Capture value by reading CCR2 register */

    /* CCR2 regsiter contains how much time the signal remained at high level */

    IC2Value = TIM1_GetCapture2();

clock_frequency = CLK_GetClockFreq();

    /* Duty cycle computation */

    SignalDutyCycle = ((uint32_t) IC2Value * 100) / IC1Value;

    /* Frequency computation */

    SignalFrequency = (uint32_t) (CLK_GetClockFreq() / IC1Value);

if(SignalFrequency>4999){

GPIO_ToggleBits(GPIOE,GPIO_Pin_7);}

  }

  else

  {

    SignalDutyCycle = 0;

    SignalFrequency = 0;

  }

  /* Clear TIM1 Capture compare interrupt pending bit */

  TIM1_ClearITPendingBit(TIM1_IT_CC2);

TIM1_ClearFlag(TIM1_FLAG_CC1);

TIM1->CNTRH = 0;

TIM1->CNTRL = 0;

enableInterrupts();

}

One last question: what should be the correct value in the IC filter?

Thanks,

Gilberto

#stm8-microcontrollers
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0