STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reset keeps occuring after program started.

Posted on May 20, 2012 at 09:43Hi, I have just received my discovery board and started to port my code over it but encountered the following problem : if I put a breakpoint at the entry point (first line of code of ''main'' function), I noticed that...

laxer3a by Associate
  • 742 Views
  • 2 replies
  • 0 kudos

Alternate function remapping, OPT bytes, and PWM2

Posted on May 24, 2012 at 16:39 Hi again, i'm trying to set a pin to an alternate remapping pin, exactly i'm using TIM2 with PWM and i want channels in D2, D3 and D4. I have tried with this: #define OPT2 0x4803 FLASH_Unlock (FLASH_ME...

pedro23 by Senior
  • 850 Views
  • 2 replies
  • 0 kudos

Passing -CP to the raisonance linker in STVD

Posted on May 23, 2012 at 16:11The linker is not case sensitive unless the -C flag is used on the command line Does anyone know how to pass this flag from within ST Visual Develop?  I can't just add -C as a user flag as STVD already passes -P and to...

Capacitive Proximity Sensor

Posted on May 18, 2012 at 14:22Hello, I need to built a capacitive proximity sensor with a range of at least 3''. What is the best sensor/controller that you advise me to use? I have been reading some things about STM8T143, but it's not easy to buy ...

paulo by Associate
  • 694 Views
  • 1 replies
  • 0 kudos

UART3 in STM8S207 with HSE

Posted on January 09, 2012 at 10:54 Please help me about I use STM8S207 for HSI : I use UART3. I can be control it normally. with follow code --> UART3_DeInit(); UART3_Init((u32)9600, UART3_WORDLENGTH_8D, UART3_STOPBITS_1,UAR...

STVD problem! It gets really slow when compiling

Posted on May 10, 2012 at 14:25Hi,Im using STVD v 4.2.1 patch 2 on my STM8 project, the problem is when I want to compile, it gets stucked annoyingly for around 10 seconds then it starts to save first and compile the codings normally. I couldnt mana...

konay61 by Associate II
  • 907 Views
  • 2 replies
  • 0 kudos

STM8S-discovery

Posted on May 10, 2012 at 16:07bonjour ,je travaille à STM8S-discovery en utilisant STVD je reçois toujours cette erreur lorsque vous essayez de démarrer une version de débogage:Starting debug session...-> Emulator reset (usb://usb)...done.Openi...

Firmware Helpfile

Posted on May 08, 2012 at 10:45Hello ST-Community, I'm searching for a special STM8S-firmware-helpfile. In this file all firmware-functions are listed with arguments etc.. I already downloaded this file a while ago. But I can't find it now. I hope s...

ldues by Associate
  • 924 Views
  • 2 replies
  • 0 kudos