cancel
Showing results for 
Search instead for 
Did you mean: 

Output Size in IDE (ROM & RAM Usage)

MuratUrsavas
Associate III
Posted on May 18, 2012 at 10:20

Hi everyone,

I can't find a solution to a very simple problem. STVD does not show the output size (ROM and RAM usage) when I compile with Cosmic Compiler (32K limited version). I tried many things and can see the output size in the generated map file. But I want to see it in the ''Build'' tab of STVD.

Is there any way to see it after a successful compilation?

Thanks in advance.

Toolchain:

IDE: STVD v4.3.1

Compiler: Cosmic STM8 32K v4.3.7

Debugger: ST-Link V2+

#stvd-cosmic-compiler-stm8l
13 REPLIES 13
MuratUrsavas
Associate III
Posted on August 01, 2012 at 16:10

Your welcome.

thibaut2
Associate II
Posted on August 10, 2012 at 14:56

Thanks a lot ! This thread was really helpful :)

n_
Associate II
Posted on January 03, 2014 at 12:57

Thank you sir it's helped me.

yanjingchang
Associate
Posted on June 24, 2015 at 07:04

Thanks a billion! Your instruction do help me a lot.