2012-10-05 8:56 AM
Hello,
when i power the stm8l1512c6 on the stm8l discovery board the microcontroller wakes up immediately after entering sleep mode. this does not happen when i power the microcontroller by the power supply. In my program the mc has to stay in halt mode for 50 seconds but when i connect the battery to the 3.3V pin on the stm8l discovery board the microcontroller goes into halt but does not stay and immediately wakes up. This seems very strange . I even cleared all external interrupt flags to make sure no interrupt is causing this although the voltage at pin 3.3V should not cause any interrupt.Any idea why this happens with a power source other than a power supply( i use a typical hameg power supply) . i can see the mc waking up immedialtly after entering halt mode when a supercapcitor or a battery is used. Should i use some capacitors from Vcc to gnd. I am not using these as they are implemented in the board itself.i use jp1 pin 1 and 2 to measure the supply current and it is always in mA since the mc is waking up as soon as it enters halt. for the battery i use a thinergy thin film battery (of course i regulate the volktage to 2 V using an ldo) and as capacitor, a .33 F supercapacitor .Any idea why this this is happening?thanks