cancel
Showing results for 
Search instead for 
Did you mean: 

is this the right code to low power for stm8l152

David.Cheng
Associate II
void main(void)
{
    
    float temperature = 0;
    const float Rp=10000.0;             //10K
    const float T2 = (273.15+25.0); //T2 298.15
    const float Bx = 3380.0;              //B
    const float Ka = 273.15;
    float Rt = 0;
    //double d_num = 0;
    float ln_value = 0;
    
    int tmp_int1 = 0;
    int tmp_int2 = 0;
    float tmp_frac = 0;
    int record_cnt = 0;  // record counter
    
    
    //uint16_t read_cnt = 2;
    //short int rd_data = 0;
    
    uint16_t k_addr = 0;
    
    //write to eeprom temperature
    
    
    CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_8);
    
    
    //CLK_GetClockFreq(void)
    //GPIO_Init(GPIOA, GPIO_Pin_2, GPIO_Mode_Out_PP_Low_Slow); // for test
    
    //TIM1_Config();
    
    LCD_Cmd(DISABLE);
    CLK_PeripheralClockConfig(CLK_Peripheral_LCD, DISABLE);
    RTC_Config();
    //ADC1_setup();
    
    //PE7
    
    
    
    
    
 
    
    
    
    while(1)
    {
        
        
        
        
        
        RTC_SetWakeUpCounter(SAMPLE_TIME * 60);
        RTC_WakeUpCmd(ENABLE);
        
        
        LCD_Cmd(DISABLE);
        CLK_PeripheralClockConfig(CLK_Peripheral_LCD, DISABLE);
        //TIM1_Cmd(DISABLE);
        //TIM1_SetCounter(0);
        //sEE_DeInit();
        
        
        
        //printf(VERSION);
        
        
        
        
        
        //PWR_UltraLowPowerCmd(DISABLE);
        halt();
 
        RTC_WakeUpCmd(DISABLE);
        //RTC_ClearITPendingBit(RTC_IT_WUT);
        
        
        
        
       
      
    }
}

we measure 70-80uA

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0