Skip to main content
TheUser
Associate II
September 26, 2020
Question

Is there a way for the STM8L DAC to retain its output voltage without drawing 80 uA during Halt mode?

  • September 26, 2020
  • 0 replies
  • 1162 views

I'm using Comparator 2 on the STM8L151G4 with DAC1 on the inverting input. When the DAC outputs 0V, the current draw during Halt mode is < 1 uA. If the DAC outputs around 0.5V before the program enters Halt mode, the current draw is 80 uA in Halt mode. Is there any way the DAC output voltage can be maintained during Halt mode and draw less current?

This topic has been closed for replies.