cancel
Showing results for 
Search instead for 
Did you mean: 

Introducing more STM8 devices with low pin count?

Philipp Krause
Senior III
Posted on July 16, 2018 at 09:32

ST has recently introduced 8-pin STM8 devices, while previously the lowest pin count available was 20.

I would like to see more STM8 devices with relatively low pin count, e.g. 12 or 14 pins. Since I intend to replace an Elan Microelectronics EM78P153A �C by an STM8, a compatible pinout would be great, but any 12- or 14-pin device would be good.

Are there any plans to introduce further STM8 devices with less than 20 pins?

Philipp

#stm8s001 #em78p153a #low-pin-count #new-device
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Bumping to remove from the home page (No Answer Posts)

ST has sale staff/organization that can provide customers with forward looking and roadmap information. Call the local office, or your distributor

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..