2009-12-09 11:42 PM
I2C bus
2011-05-17 6:02 AM
I work stm8205k6 chip and i need to drive i2c bus
on standard mode & master mode. power supply is 3v and fclk is 4.096 mhz. can i2c bus drive with this supply? I init GPIOB port to reset value at first program.and use pull up resistor on SDA &SCL lines but busy bit in the SR3 register always set to 1 and not allow to do start condition! it clear when swrst bit in CR2 register set to 1.i don't know how to do! i use ride7 IDE version 7.14 & Rkit-stm8 version 2.13.2011-05-17 6:02 AM
Hello,
the reference stm8205k6 does not exist for other questions : The I2C can be drived by power supply 3V and Fclk 4Mhz I advice you to use 4K7 ohm as value for pull up resistor Best Regards Bassinux2011-05-17 6:02 AM
Hi
thanks for your help 1.what does means ''reference stm8205k6 doesn't exist '' don't i continue to work it and change my chip? can i use the stm8207k6 chip? 2.I used 4K7 ohm resistor on SDA & SCL lines but cannot drive i2c bus. my init i2c function is in below: { I2C->CR1 &= ~(0x01); //disable PE I2C->FREQR = 0x04; I2C->CCRH |= 0x00; I2C->CCRL |= 0x14; //fclk 100000hz I2C->TRISER |= 0x05; I2C->CR1 |= 0x01; //PE enable I2C->OARH |= 0x40; } when send init function, busy bit set to 1. then send start condition.but any happend on i2c lines!2011-05-17 6:02 AM
Hi,
1) Regarding to the ST web site there is no chip with this name stm8205k6, the correct one is stm8207k6, this is which I mean by Reference. 2) Concerning your application it seems correct but I suggest to let the PE Enable the Last instruction. After sending Start condition verify if SB flag in SR1 is set to 1. be carefull in I2C pins mapping, verify if works with the correct package Best rergards Bassinux2011-05-17 6:02 AM
Hi
I checked the SB flag in SR1 register, it isnot set to 1 after sending start condition. i don't heve stm8s207k6 chip and still work with stm8s205k6.is it possible 205k6 chip- i2c module have problem? thanks and best regards2011-05-17 6:02 AM
Hi
11 & 12 pin numbers(PB4 & PB5) are SDA & SCL lines of i2c bus in the stm8s205k6 chip (32 pins). is it ok?2011-05-17 6:02 AM
Hello I.yeganeh,
I suggest you to check the pinout.2011-05-17 6:02 AM
hi, the stm8s205k6 is the current STM8S105K6
regarding the problem, did you tested your application-hardware with the I2C example on the library? this is the quickest way to know if there is something wrong with your mcu. BTW, try using the 16Mhz configuration at first. I've had some issues when using the clock at 24Mhz2011-05-17 6:02 AM
Is this issue been resolved? I have the exact same behavior with the STM8S105K6. The SR3 Busy bit is always settled even if SCL and SDA pins are high level.
Thanks,
Mat