cancel
Showing results for 
Search instead for 
Did you mean: 

How to do RTC calibration (STM8L151F3)

Leo1986
Associate II

Hi,

I am using RTC in WakeUp mode to wake the MCU to save energy.

The problem is that the RTC time base is not accurate as I am using LSI on the RTC.

Is there any way to make RTC more accurate using LSI as a clock source?.

CLK_PeripheralClockConfig(CLK_Peripheral_RTC, ENABLE);          

CLK_RTCClockConfig(CLK_RTCCLKSource_LSI, CLK_RTCCLKDiv_1);        

RTC_WakeUpCmd(DISABLE); 

if( RTC_GetFlagStatus(RTC_FLAG_WUTF) == SET )

{

     RTC_ClearITPendingBit(RTC_IT_WUT);

}

  // LSI               = 38kHz   (LSI)

  // LSI/16              = 2375kHz (Preescaler 16)

  // Timer_Resolution = 1/(2375kHz) = 421,0526us  

// periodicEvent = Timer_Resolution*238 (100ms)

    

  RTC_SetWakeUpCounter(238);    // 100ms            

  RTC_WakeUpClockConfig(RTC_WakeUpClock_RTCCLK_Div16);     

  RTC_WakeUpCmd(ENABLE);

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0