STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stvd newbie

I've generated an output file from STVD in .elf format. But stvp requires motorola hex format. Do I have to do another conversion?

Elong.1 by Associate II
  • 713 Views
  • 2 replies
  • 0 kudos

Is there an 8-bit USB with HS or 3.0 USB MCU?

I found that the ST72681 8-bit MCU has HS function. Do you still support this MCU? Or is there a related follow-up product?Looking forward to your message​

HHo.2 by Associate
  • 493 Views
  • 0 replies
  • 0 kudos

STM8AL3LE88 debug connection error

I trying to debug STM8AL3LE88. There is no problem with STVP in reading and writing device memory and option bytes. But in STVD when i Start Debug it ends with error warning:Starting debug session... -> Emulator reset (usb://usb)... ** Connection err...

STM8L151 USART not Sending, any Ideas why??

Hello Everyone,This problem is persisting. I am using the STM8L151 Standard Peripheral Library to send an array of bytes over USART1. Code executes, but i see nothing on the Pin (using Oscilloscope), nor can i see the Data Rigister changing (Using ST...

AHama.1 by Associate
  • 547 Views
  • 0 replies
  • 0 kudos

STVD an anomaly (1) has been detected during installation?

The only thing which I can offer is at the end of the install when continuing from the display release notes page it hangs. I tried leaving it a while but the only way to exit is to close the program via task manager.Any suggestions?Thanks.

Hi I use STM8L050J3. I have problems with the IDE's:

IDE's:1. IAR - I succeed complying the project but when trying debugging it (with SWIM + ST-LINK2), I get the error message: "Failed to set configuration with MCU name STM8L051F3: SWIM error [30006]: Comm init error: chip does not answer."In the Tar...

Ofer by Associate III
  • 550 Views
  • 0 replies
  • 0 kudos

I2C slave configuration for STM8S208RBT6

Hello, I am trying to use STM8S208RBT6 as an I2C slave. It seems to be configured correctly, yet it doesn't acknowledge its address, and it doesn't get an interrupt. The registers are as follows:PE_DDR = 0x20;PE_ODR = 0x20;PE_CR1 = 0x20;PE_CR2 = 0x...

EBogo.1 by Associate II
  • 673 Views
  • 1 replies
  • 0 kudos

EEPROM on STM8L001

HelloI wonder if there is some example code available on how to use the Data EEPROM in the 8pin STM8L001J3.I did successfully work with the internal Data EEPROM on the STM8L051, but no success on the SO8. The address I used is 0x9BFB (in contrast to ...

How to do RTC calibration (STM8L151F3)

Hi,I am using RTC in WakeUp mode to wake the MCU to save energy.The problem is that the RTC time base is not accurate as I am using LSI on the RTC.Is there any way to make RTC more accurate using LSI as a clock source?.CLK_PeripheralClockConfig(CLK_P...

Leo1986 by Associate II
  • 588 Views
  • 0 replies
  • 0 kudos