2010-08-02 11:19 PM
Hello.
I've read on another forum that the Discovery board has the incomplete version of ST-LINK that can program only s105c6 and nothing else via SWIM. Please confirm or deny this information. Can Discovery be used for programming STM8L and other STM8S controllers ?2010-08-03 05:21 AM
Hello ,
With this embeded version of STLink you are ablle to program all STM8 devices (S,L & A). The only limitation is with voltage level for STM8L devices . No voltage adapter has been added in this version so 1.8V is not supported. STM32 devices are not supported. Best Regards Grom