cancel
Showing results for 
Search instead for 
Did you mean: 

Desoldering the sockets

infoinfo968
Associate II
Posted on August 28, 2010 at 12:18

I'd like to make the board more useful by desoldering the header plugs on the board and replacing them with sockets I can plug wires directly into.

I've tried using braid and my solder sucker but neither is working effectively. Does anyone have any advice for removing these plugs ? Or am I better off using sockets and headers and so on ?

3 REPLIES 3
johnstrong
Associate
Posted on August 28, 2010 at 19:33

Paul,

Try using a little solder on the connections first, The flux in your solder is often better than the flux on cheap desoldering wicks, also your solder will likely have a lower melting point than the boards. then use your solder puller.

Personally, I'd leave the board along and use female jumpers, such as those made by Schmartboard.

John

infoinfo968
Associate II
Posted on August 30, 2010 at 03:08

Thanks - I'll look those connectors up :)

RomainR.
ST Employee
Posted on September 21, 2010 at 09:50

Paul,

Personally, I unsolder the 2x6 male header that I replaced by females on the copper side.

No trouble for it with a little iron and a pump

In this way, the board can be plug over an extension and i can access to all IO pin.

romain

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.