2015-11-17 10:54 PM
Hello,
We had developed one application using STVD IDE & cosmic compiler with 8k limit, for that we have following error while compile the code.#error clnk Release\stm8s003.lkf:1 segment .text size overflow (1358)
The command: ''clnk -l''C:\Program Files\COSMIC\32K_Compilers\CXSTM8\Lib'' -o Release\stm8s003.sm8 Release\stm8s003.lkf '' has failed, the returned value is: 1exit code=1. Now we have cosmic compiler with STM8_STM32_32k license.lic file which is copied into License folder & then compile the code but still we have same error as above so please help us & give solution.Thank You.2015-11-18 12:20 AM
2017-03-19 11:49 PM
can you please tell me how to overcome this problem.
I also had the 32k license file
2017-03-22 1:33 AM
Hi,
download the latest free version from the Cosmic website that has no (more) code size limit and the problem will go away.
Regards,
Luca
2017-03-22 2:07 AM
hi
I have installed the latest version only, cxstm8_FSE_stm32_32K I'm using