cancel
Showing results for 
Search instead for 
Did you mean: 

compiling ok but non funktional code

andreaskramer9
Associate
Posted on December 08, 2011 at 00:42

Hi,

first sorry for my english (its not my native language).

I have a problem getting funktional code for an STM8S005C6 ( eval Board ).

I use the STVP with Raisonance C compiler and i am able to compile code without errors.

Very simple code pieces work ( like a blinking Led ).

But there seems to be an error with the clock. When i toggle a pin in a while(1) construct i can only meassure aprox 300 kHz frequency at the pin.

I think this should be much higher since systemclock is configured as HSI with devider 1.

Next thing is i can´t bring the sample prog ( AN3996 ) to work.

It compiles without errors but when i upload it an reset the board it isn´t working. The led is on the whole time without any reaction to the touch button.

My last try was to write a programm to communicate with the uart1. But it never sends anything. My programm is stuck at this part:

  /* Write X to the UART1 */

  UART1_SendData8('X');

  /* Loop until the end of transmission */

  while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET)

  {

   GPIO_WriteReverse(GPIOD, GPIO_PIN_0);

   //It never leaves this loop

  }

The whole main.c is in the attachment. The other files are from the Project_template (AN3996).

Maybe anyone can give me a clue where to search or what to change that i can produce working code for the STM8S.  ( Oh i totaly forgot to mention that i can reupload the original working hexfile so it seems to be no hardware bug )

Greetings A.Kramer

EDIT: I found the source of my problem. The target declaration wasn´t the same in STVD and the makefile. There was a hidden wrong target and all code was compiled for the wrong device.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0