2016-07-29 4:54 PM
I'm sorry for my bad in English.
[STVD + COSMIC_C : STM8S103K3]I want to use prototype function which need EXECUTION_FROM_RAM.after i build.. It ERROR..!!help me please.. T_T!// ------------------------ below.. is stm8s_flash.c (stm8s.. StdLib) -------------------------------//Steps of the execution from RAM differs from one toolchain to another:
- For Cosmic Compiler: 1- Define a segment FLASH_CODE by the mean of '' &sharppragma section (FLASH_CODE)''. This segment is defined in the stm8s_flash.c file. 2- Uncomment the ''&sharpdefine RAM_EXECUTION (1)'' line in the stm8s.h file, or define it in Cosmic compiler preprocessor to enable the FLASH_CODE segment definition. 3- In STVD Select Project\Settings\Linker\Category ''input'' and in the RAM section add the FLASH_CODE segment with ''-ic'' options. 4- In main.c file call the _fctcpy() function with first segment character as parameter ''_fctcpy('F');'' to load the declared moveable code segment (FLASH_CODE) in RAM before execution. 5- By default the _fctcpy function is packaged in the Cosmic machine library, so the function prototype ''int _fctcopy(char name);'' must be added in main.c file.// ---------------------------------------------------------------------------------------------------------//Step 1 , 2 , 4 and 5 , i make done.but i confuse step 3..//----------------------------------------------------------------------------------------------------//3- In STVD Select Project\Settings\Linker\Category ''input'' and in the RAM section
add the FLASH_CODE segment with ''-ic'' options//----------------------------------------------------------------------------------------------------//[url=http://www.uppic.org/share-479C_579BEACC.html][img]http://www.uppic.org/image-479C_579BEACC.jpg[/img][/url]when build..//------------------------------------------------------------------------------------------------------//clnk -l''C:\Program Files\COSMIC\FSE_Compilers\Lib'' -o Debug\stm8s103.sm8 -mDebug\stm8s103.map Debug\stm8s103.lkf
&sharperror clnk Debug\stm8s103.lkf:1 segment .FLASH_CODE size overflow (161) The command: ''clnk -l''C:\Program Files\COSMIC\FSE_Compilers\Lib'' -o Debug\stm8s103.sm8 -mDebug\stm8s103.map Debug\stm8s103.lkf '' has failed, the returned value is: 1exit code=1.stm8s103.elf - 3 error(s), 0 warning(s)//------------------------------------------------------------------------------------------------------//How do i solve this problem..? #stm8s-cosmic_c-execution_ram