Skip to main content
pietruha8
Associate II
June 20, 2011
Question

.bsct size overflow (discovery, cosmic)

  • June 20, 2011
  • 3 replies
  • 1958 views
Posted on June 20, 2011 at 22:53

Hello everyone,

I've got problem with compilation of my application

Running Linker

clnk -l''C:\Program Files\COSMIC\CXSTM8_16K\Lib''  -o Debug\stvd_project.sm8 -mDebug\stvd_project.map Debug\stvd_project.lkf

#error clnk Debug\stvd_project.lkf:1 segment .bsct size overflow (296)

#error clnk Debug\stvd_project.lkf:1 segment .ubsct size overflow (10)

 The command: ''clnk -l''C:\Program Files\COSMIC\CXSTM8_16K\Lib''  -o Debug\stvd_project.sm8 -mDebug\stvd_project.map Debug\stvd_project.lkf '' has failed, the returned value is: 1

exit code=1.

Is there anyone that can help with this problem?

Thank you in advance.

    This topic has been closed for replies.

    3 replies

    Andrew Neil
    Super User
    June 20, 2011
    Posted on June 21, 2011 at 00:04

    Have you tried looking up .bsct and  .ubsct in the Cosmic manual?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    jdf25252
    Associate II
    June 21, 2011
    Posted on June 21, 2011 at 16:54

    okelm

    First thing see my response to Nico on Memory use and allocation.

    .bsct & .ubsct are zero page sections & there is only 256 bytes available there. 

    You should check your memory model.  I suspect that you're using ''Short Stack (+mods0)''  This model's default variable placement is into the zero page.  I would suggest using ''Long Stack (+modsl0)''.  This memory model will place all variables into the .data & .bss segments which should give you about 1.5K bytes for your variables.

    jdf

    pietruha8
    pietruha8Author
    Associate II
    June 29, 2011
    Posted on June 30, 2011 at 00:07

    ok, thanks ;] problem solved