Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.
ic STM8L052C6, Programmer ST Visual developer, ST Visual programmer and writing through ST LINK V2
Posted on January 14, 2018 at 09:04 Hi All, I am new to STM8S and not yet that good at microcontroller programming in general. I am trying to learn about timers/counters in microcontrollers. I wrote following code to toggle an LED connected...
Determine FLASH areaDue to its file extension (or lack thereof), "C:\Users\HARISH~1\AppData\Local\Temp\arduino_build_202135/DigitalInputPullup.ino.hex" is considered as INTEL HEX format!2596 bytes at 0x8000... Tries exceededAn error occurred while up...
I have an STM8S00f3p6 controller I was able to do the external interrupt and do the GPIO operations in the interrupt.Now my requirement is like after getting the inerrupt I need to make two GPIOS high for some seconds and make them down after time ex...
I have downloaded and installed the cosmic(CXSTM8).I have tried to compile the code,but that time I have faced the license error. Please find the attachment .kindly help me out.
1. I have to read/write NAU7802 register, datasheet of which is attched.2. STM8S is running at 16Mhz.3. Write three functions:a) i2c_init() : init the i2c peripheralb) i2c_read_one_byte_data() : read from address of NAU7802 and read only one bytec) i...
I need a clock signal for my hardware that occurs in the middle of each uart tx bit. But I don't want the synchronous mode behavior where receives are based on transmits. I want receives to start when start bits are received on the uart rx pin, whi...
HiI need to migrate my working STM8S003F3P6 code (working correctly for a year now) to a new STM8L051F3 chip.(The code is SDCC compiled and bit banged with direct register modification. I do not use the SPL) I run an interrupt at 125Hz on Timer2 in t...