STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

power draw when stopped STM8Lxxx

hi alli am first time user to ST micros. (8bit motorola mostly)I am looking at using stm8L132r8 in an ultra low power device, which needs 10year battery life.the micro will be stopped most of the time, woken by the RTC running from external 32khz xta...

dwood.1 by Associate
  • 567 Views
  • 0 replies
  • 0 kudos

BLDC Motor controller

I am new and novice can some one guide for using STM8Sxxx three-phase BLDC motor control software library V1.0. From the manual I am unable to build. Is there a tutorial or example on it. Looking for closed loop250W 36V Motor.

VSaha by Associate
  • 593 Views
  • 0 replies
  • 0 kudos

STM8AF6213PDU TIM5 and ADC1 library problem

I am using STM8AF6213 MCU in my project. I am using PD6 (AIN6) pin to read analog value. I use PD4 (TIM5_CH1) to generate PWM. But the stm8_adc1.h and stm8_tim5.h libraries that I included in my project do not work properly. It does not see the funct...

0693W000003QcmvQAC.jpg 0693W000003QcmlQAC.jpg
OOzde.2 by Associate
  • 517 Views
  • 0 replies
  • 1 kudos

What does the STM8 TIM3_BKRConfig() function do?

As a newbie I'm struggling to understand the following line of code:TIM3_BKRConfig(TIM3_OSSIState_Enable,TIM3_LockLevel_1,TIM3_BreakState_Enable,TIM3_BreakPolarity_High,TIM3_AutomaticOutput_Enable);Introductory material that I've found on timers/PWM ...

PiSquared by Associate II
  • 1132 Views
  • 1 replies
  • 0 kudos

STM*S-discovery with st8ms105c6t6 mcu -- I am going nuts

I have an asm program written in ST Visual develop. Using stvd, and updloading to a STMS103f3, it runs fine. Change the target in ST v develop and build it and upload to the discovery bd thru it's st-link, it doesn't run. Checking the register add...

JTann.1 by Associate II
  • 780 Views
  • 0 replies
  • 0 kudos

STM8S005K6 Bootloader no responding at data

HiI have a problem when I start writing the first page of the program.I am running at 115200 8 data bit, 1 stop, no parity.I am running in ECHO mode, meaning I return all bytes from the bootloader.I have send the SYNC byte, at power up, and getting a...

HMoel.1 by Associate II
  • 844 Views
  • 2 replies
  • 0 kudos

Please help me reverse engineer these buttons...

Hi,I am trying to figure out how a set of buttons interfaces with the microprocessor - an STM8S 003K3T6C ([url=https://www.st.com/resource/en/datasheet/stm8s003f3.pdf]datasheet[/url])I am familiar with simple button config - you pull GPIOs high or lo...

Rjohn.1 by Associate II
  • 1763 Views
  • 5 replies
  • 0 kudos