STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm8s003k3 multiple ADC channel reading error

Hi everyone.I am having problem reading data on ADC pins in stm8s003k3. I have attached three NTC at Ain1/2/3(which I suppose is also known as a channel) according to the datasheet. Problem is that when I put different channels in my code it shows on...

KRiaz.1 by Associate II
  • 1021 Views
  • 1 replies
  • 0 kudos

Resolved! conditional transition to sleep mode

In many aplications i am using simple template, where interrupt routines (for example UART receive) raise flags (volatile variables) and main() function polling these flags and processing these events (for example parsing incoming UART charaters). I ...

How disable VrefInt ?

Hi there,On a battery-powered board using the STM8l050J3, in order to reduce at the minimum the power consumption, in Active Halt mode and using RTC wakeup, (at a few tens or at most hundreds of uA) as indicated, I want to disable Vrefint.To do so, d...

Would writing to same flash address reduce lifespan of MCU

I am using STM8 and since vector table is in flash memory I need to write to flash memory in order to create and use vector table. Since addresses of vector tables are fixed my code writes same values to same memory address of the flash on every star...

GunkutA by Senior
  • 1046 Views
  • 1 replies
  • 0 kudos

VL53L1x communication with STM8S105 MCU

Dear all,I have just put the X-NUCLEO-53L1A1 kit into operation together with Arduino UNO and everything works perfectly, using the "X_NUCLEO_53L1A1_HelloWorld" application package.Then I mounted one of the same two VL53L1X-SATEL sensors by interfaci...

0693W00000Kc552QAB.jpg 0693W00000Kc5OiQAJ.bmp 0693W00000Kc5P7QAJ.bmp
CCenc.1 by Associate
  • 2043 Views
  • 3 replies
  • 1 kudos