STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM8L151G3 TIM4 not working

MCU: STM8L151G3U6ISSUE: TIM4 interrupt doesnt seem working Connections:                 1. LED on pin PB0                 2. Push button/ switch on pin PC5Scenario:1. User press the push button2. Toggles the LEDObservation:Without using the TIM4 inte...

zin10 by Associate II
  • 2299 Views
  • 1 replies
  • 1 kudos

stm8 using AWU/HALT/EXTI

I am building time lag switch- i have at42q1010 touch ic connected to PA3- i have stm8s003f3 mcu- Using latching relay to conserve power- timeout is my pot value- Exti on at42q1010 rising edge exti_cr1 =0x01; ( the ic reads low when no touch and when...

mag1_eng by Associate
  • 2306 Views
  • 0 replies
  • 0 kudos

Resolved! STM8S103 Timer TIM2 timing

Hi,Using ST Workbench debugger my 16-bit timer TIM2 (china bought) overflows each 16 seconds as the prescaler is set to 10. With an 16MHz internal clock divided by 2^10 (1024) the timer should overflow theoretically each 4.1 seconds. Prescaler 9 take...

sthvw by Associate III
  • 1413 Views
  • 9 replies
  • 1 kudos

Resolved! Can't get grip on PA1 interrupt

Hi,I fell in love with this cute little uC and created all kinds of succesfull projects.Now I have a problem. I want to decode DCF77 time signals. I bought me a few DCF77 receivers from China. They all work fine. I connected the data output of the DC...

sthvw by Associate III
  • 559 Views
  • 1 replies
  • 0 kudos

Resolved! STM8 SWIM Debug Protocol

Hello,I’ve been working on implementing a SWIM master using an STM8 device to interface with a STM8S105K6 target. This is part of a tester software project that was previously using the ST7 debug protocol and is now being ported to the STM8.I’ve foll...

andryas_mariotto_0-1749051883648.png

Resolved! Save data to EEPROM after VDD drops

Hello!Is it possible to save data to EEPROM in STM8S001J3 after VDD drops (power outage)?I would appreciate any case indication. I appreciate any help in advance.

Vladix by Associate
  • 530 Views
  • 2 replies
  • 2 kudos

NEC protocol based remote with STM8S105K4T6

I am trying to make a project using STM8S105K4T6 and NEC based IR remote. I am using Sduino to program the board. I want to turn on and off two relays and two leds using IR remote. Please help me to make the IR decoder for the board. 

RV97 by Associate
  • 692 Views
  • 3 replies
  • 0 kudos

STm8S001J3 Bandgap

Hi,  please, I'm looking how to program  STMS8001J3 in order  to  generate a reset using bandgap (AIN7) reference voltage. Thanks.