STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STVD displays ''The parameter is incorrect''

Posted on March 26, 2011 at 04:17Just received my STM8L-Discovery, installed STVD 4.2.1 and Raisonance compiler. Whenever I hit F7, STVD shows this non-descriptive message ''The parameter is incorrect''. After that, the only way to exit the applicat...

EXTI not work correct

Posted on August 04, 2011 at 08:53When I use PA6,PD6 is EXTI_Trigger_Rising_Falling.When PA6 go H-->L, it generate interrupt, but When I keep PA6 still Low, and PD6 go H-->L, it not generate interrupt. Please help me. void main() {     CLK_SYSCLKDiv...

np1 by Associate II
  • 839 Views
  • 4 replies
  • 0 kudos

stm8l, eeprom, dma - problem of access

Posted on June 06, 2011 at 11:56 If writing (erasing) byte(word, block) in the eeprom memory, DMA transaction occurs on the periphery of RAM (tested only this type of transfer) of the microcontroller hangs (not working). The documentation no found ...

Software simulator.

Posted on August 02, 2011 at 19:30I'm trying to us the software simulator to simulate the 207S6 but the internal registers don't seem to be working correctly. The reset value are all ff's. The ADC doesn't seem to function as well as the timers anyon...

u32 =u16*u16

Posted on July 30, 2011 at 02:39Never used the Cosmic complier before do I require any header like math.h to do a u16*u16 into u32 doesn't seem to do anything.

HSE Config

Posted on July 25, 2011 at 17:35I need to config my stm8s105k6 to work with oscillator of 16Mhz my code : CLK_ClockSwitchCmd ( ENABLE );  CLK->SWR  = 0xB4;  CLK->SWR  = 0xB4;  while ( !(CLK->CMSR == 0xB4 ) ); I get stuck behind the while loop Am I m...

greg_t by Associate II
  • 673 Views
  • 1 replies
  • 0 kudos

DATA EEPROM area - problem writing byte

Posted on July 12, 2011 at 13:13Hi experts, in my application I am trying to write a single byte to an address in the DATA EEPROM area immediately after disabling ''the DATA area write protection by writing consecutively .. MASS keys to the FLASH_DU...

No stm8s103 in ''STVD\settings\MCUselection list

Posted on July 19, 2011 at 14:29Hi.   No stm8s103 in ''STVD\settings\MCUselection list It start with stm8s207 I have cosmic 16 k free compiler additional problem is ''#error clnk Release\rtos_osa_hw.lkf:1 no default placement for segment .info.''...

slava by Associate
  • 544 Views
  • 1 replies
  • 0 kudos

Upgrading to the STM8 Assembler question

Posted on July 04, 2011 at 09:33After having written a time consuming and reasonably eloquent request about this subject, only to have it rejected and erased, I'll make a shorter attempt. Is it not possible to have straight forward assembler templat...