2011-03-29 10:03 AM
Hi All,
I have taken some of the sample code that comes with the stm8l-discovery eval board to try and talk to hyperterm on from stm8. when i try to send anything all I see is garbage on the hyperterm screen... I have verified both side have the same settings, 115200, no polarity, 1 stop bit, 8 bit word length - butstill it does not work. Can I get some help to get this working? My sample code snippet is as follows - can someone explain what I am doing wrong? &sharpdefine DBG_COM1 USART1 &sharpdefine DBG_COM1_GPIO GPIOC &sharpdefine DBG_COM1_CLK CLK_Peripheral_USART1 &sharpdefine DBG_COM1_RxPin GPIO_Pin_2 &sharpdefine DBG_COM1_TxPin GPIO_Pin_3 &sharpdefine DBG_COM1_ClkPin GPIO_Pin_4 typedef enum { COM1 = 0 } COM_TypeDef; USART_TypeDef* COM_USART[COMn] = { DBG_COM1 }; GPIO_TypeDef* COM_PORT[COMn] = { DBG_COM1_GPIO }; const uint8_t COM_USART_CLK[COMn] = { DBG_COM1_CLK }; const uint8_t COM_TX_PIN[COMn] = { DBG_COM1_TxPin }; const uint8_t COM_RX_PIN[COMn] = { DBG_COM1_RxPin }; const uint8_t COM_CLK_PIN[COMn] = { DBG_COM1_ClkPin }; static void COMInit(COM_TypeDef COM, uint32_t USART_BaudRate, USART_WordLength_TypeDef USART_WordLength, USART_StopBits_TypeDef USART_StopBits, USART_Parity_TypeDef USART_Parity, USART_Mode_TypeDef USART_Mode) { USART_DeInit(COM_USART[COM]); /* Enable USART clock */ CLK_PeripheralClockConfig((CLK_Peripheral_TypeDef)COM_USART_CLK[COM], ENABLE); /* Configure USART Tx as alternate function push-pull (software pull up)*/ GPIO_ExternalPullUpConfig(COM_PORT[COM], COM_TX_PIN[COM] | COM_RX_PIN[COM] , ENABLE); /* USART configuration */ USART_Init(COM_USART[COM], USART_BaudRate, USART_WordLength, USART_StopBits, USART_Parity, USART_Mode); } main() { ... COMInit(COM1, (uint32_t)115200, USART_WordLength_8b, USART_StopBits_1, USART_Parity_No, USART_Mode_Tx | USART_Mode_Rx); USART_Cmd(COM_USART[COM1], ENABLE); //try to send a few bytes to hyperterm USART_SendData8(DBG_COM1, 0x41); while (USART_GetFlagStatus(DBG_COM1, USART_FLAG_TC) == RESET); USART_SendData8(DBG_COM1, 0x42); while (USART_GetFlagStatus(DBG_COM1, USART_FLAG_TC) == RESET); ... when i do these writes all I see is garbage on PC hyperterm screen... My h/w setup is as follows: PC2 pin jumpered to TX on DB9 connector PC3 pin jumpered to RX on DB9 connector #usart-rs2322011-04-06 1:24 AM
In fact, if you check in the driver functions the baud rate frequency depends of CPU clock frequency. I can suggest to you to check if these points:
> Check which clock is used in your application (LSI, HSI, ...); > Check the CPU clock frequency; > Check in USART register the values setted; This is the first way .... Other points, questions: > In you application do you send the caracters one by one (place one break point after the first caracter is sent ( line: while( ....) ) and check it.? > Have you try the reception from hyperterminal? I hope that these points can help you. Best regards PhilippeHi All,
I have taken some of the sample code that comes with the stm8l-discovery eval board to try and talk to hyperterm on from stm8. when i try to send anything all I see is garbage on the hyperterm screen... I have verified both side have the same settings, 115200, no polarity, 1 stop bit, 8 bit word length - butstill it does not work. Can I get some help to get this working? My sample code snippet is as follows - can someone explain what I am doing wrong? #define DBG_COM1 USART1 #define DBG_COM1_GPIO GPIOC #define DBG_COM1_CLK CLK_Peripheral_USART1 #define DBG_COM1_RxPin GPIO_Pin_2 #define DBG_COM1_TxPin GPIO_Pin_3 #define DBG_COM1_ClkPin GPIO_Pin_4 typedef enum { COM1 = 0 } COM_TypeDef; USART_TypeDef* COM_USART[COMn] = { DBG_COM1 }; GPIO_TypeDef* COM_PORT[COMn] = { DBG_COM1_GPIO }; const uint8_t COM_USART_CLK[COMn] = { DBG_COM1_CLK }; const uint8_t COM_TX_PIN[COMn] = { DBG_COM1_TxPin }; const uint8_t COM_RX_PIN[COMn] = { DBG_COM1_RxPin }; const uint8_t COM_CLK_PIN[COMn] = { DBG_COM1_ClkPin }; static void COMInit(COM_TypeDef COM, uint32_t USART_BaudRate, USART_WordLength_TypeDef USART_WordLength, USART_StopBits_TypeDef USART_StopBits, USART_Parity_TypeDef USART_Parity, USART_Mode_TypeDef USART_Mode) { USART_DeInit(COM_USART[COM]); /* Enable USART clock */ CLK_PeripheralClockConfig((CLK_Peripheral_TypeDef)COM_USART_CLK[COM], ENABLE); /* Configure USART Tx as alternate function push-pull (software pull up)*/ GPIO_ExternalPullUpConfig(COM_PORT[COM], COM_TX_PIN[COM] | COM_RX_PIN[COM] , ENABLE); /* USART configuration */ USART_Init(COM_USART[COM], USART_BaudRate, USART_WordLength, USART_StopBits, USART_Parity, USART_Mode); } main() { ... COMInit(COM1, (uint32_t)115200, USART_WordLength_8b, USART_StopBits_1, USART_Parity_No, USART_Mode_Tx | USART_Mode_Rx); USART_Cmd(COM_USART[COM1], ENABLE); //try to send a few bytes to hyperterm USART_SendData8(DBG_COM1, 0x41); while (USART_GetFlagStatus(DBG_COM1, USART_FLAG_TC) == RESET); USART_SendData8(DBG_COM1, 0x42); while (USART_GetFlagStatus(DBG_COM1, USART_FLAG_TC) == RESET); ... when i do these writes all I see is garbage on PC hyperterm screen... My h/w setup is as follows: PC2 pin jumpered to TX on DB9 connector PC3 pin jumpered to RX on DB9 connector2011-05-31 6:38 AM
Hi,
i'm not sure, but you may need a level shifter between stm8l-discovery and PC port?