STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello world example

Posted on December 30, 2011 at 16:00 Hi there ! I am a newbiein ST microcontroller. 1) Tobeginning, I bought : * A http://www.st.com/internet/evalboard/product/251jsp (with a stm8l101K3 MCU) * A http://www.raison...

gege089 by Associate
  • 1258 Views
  • 2 replies
  • 0 kudos

stvd ver 4.3.0 not open file of project

Posted on January 05, 2012 at 18:31regards to all. I have installed stvd ver 4.3.0 and free cosmic C compiler,the problem is that  i can notopen anyfiles of the project to edit,the IDE hangs with lost functionality. There is a solution to this probl...

''Error : Cannot communicate with the board'' after some use of it

Posted on January 05, 2012 at 15:54Hello,     The SM8S-Discovery are crashing after some time of use. The ''ST Visual Develop'' give the error ''Error : Cannot communicate with the board''. After the first time that the error happens, the board beco...

mob by Associate
  • 605 Views
  • 0 replies
  • 0 kudos

STM8L-Discovery Debugging

Posted on January 21, 2011 at 08:27Hello, I use the ST Visual Develop IDE together with the Cosmic Compiler and the STM8L-Discovery. Everything seems to work fine, besides the debug function. When I try to start debugging I get the following error m...

stm8 by Associate II
  • 3931 Views
  • 10 replies
  • 0 kudos

STVD V4.3.0 Hangs on Edit

Posted on December 16, 2011 at 09:33Hi, My setup : Windows Vista STVD V4.3.0 Cosmic C compiler STM8S Discovery board I use the example project 'stm8s-discovery_led'. I have opened the '\Project\Discover\STVD\Cosmic\Discover.stw' workspace and it bui...

joost by Associate
  • 930 Views
  • 3 replies
  • 0 kudos

EXTI_SRx register

Posted on May 07, 2011 at 08:38EXTI_SRx register

asim1108 by Associate II
  • 704 Views
  • 2 replies
  • 0 kudos

USART - Data size difference problem between Reception and Transmission

Posted on November 29, 2011 at 07:59Hi,I have established a connection between dev-board and pc by rs232 and the settings are programmed like data size 8 bit long, 1 stop bit, Parity - odd, 115200 baudrate..  And when I talk to the board (receiving)...

konay61 by Associate II
  • 974 Views
  • 2 replies
  • 0 kudos

stm8s003k3

Posted on December 14, 2011 at 11:48i want to configure uart of stm8s003k3  as i have the code of uart for stm8s105c6t6 chip but when i select the stm8s003k3 chip complication  gives and error.can anyone please tell me what can i do for same code to...

STVD 4.3.0 crash

Posted on November 30, 2011 at 21:51Hello,I have a problem with STVD 4.3.0. When I try to open the workspace the program crash. Behaves the same way when I create a new project and trying to modify it in the editor. The problem appeared only in vers...