STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

soft reset for stm8s003f3

hi,i am developing a code, i want to soft reset the micro using instructions in cosmic C compiler. can any one help? 

ahp by Associate
  • 1296 Views
  • 2 replies
  • 0 kudos

STM8S103F3 programming error while using STVP

Hi All,This is my first post here and also my first interaction with ST micro devicesI'm truing to flash a .hex file into an STM8S103F3 using ST LINK V2 and STVP but I cannot connect to the device. I'm using a 5V external supply connected to the VDD ...

IMG_4109.JPG IMG_4110.JPG Capture.PNG

STM8S103F3 and OLED 128x32

Please I have mini board with processor STM8S103F3 and I need use I2C communication for OLED 128x32 panel SSD1306. Is there examples for ARDUINO IDE or STV Developer and Cosmic.Thank you very muchZdenek

Zdenek by Associate
  • 3233 Views
  • 2 replies
  • 0 kudos

two stm8s105c6t6 master and slave

Hi! i have two stm8105c6t6 , i want use one to master and other to slave, two pcb board are connect using 10k pull up resistor in the SDA/SCL line.  i am using the example AN3281 stm, but my microcontroller not have tim4, i change the tim4 to tim3 bu...

jdo by Associate II
  • 1008 Views
  • 1 replies
  • 0 kudos

Quarry About STM8S Programing Erase

Hello everyone,I am Prashant . I try to program STM8S001 microcontroller once I flash the code of UART and I initialize TX pin 8(PORT PD5) or 5(PORT PA3) after that i am trying to flash code again in controller but it's giving me SWIM Communication E...

Prashant911318_0-1695728343746.png

I set the RTC time. I call it up

I deleted the contents because I set the wrong writing label I'm sorryI can't find a place to write

ark2 by Associate III
  • 1189 Views
  • 1 replies
  • 0 kudos

Missing ZKW HaMOn Database Data

Dear Sir/MadameConcerning to our ZKW HaMOn (Hardware Management Online)Database, due to our customers' requirements, we need to have some information.Could you please mail me as soon as to send table with MPNs to have required information.Thanks for ...

Resolved! ST Visual Develop crashes when starting Tools -> Programmer

Posted on March 16, 2018 at 07:23I have been using ST Visual Develop with the STM8 Cosmic Compiler on a Virtual PC with Win10 for months.Now I want to use it on my normal PC (also Win 10 64 bit  Version 1709), CosmicCompiler is working but I cannot ...

STM8S ST VISUAL PROGRAMMER

Hi, I'm using ST VISUAL DEVELOP. An error occurs.  it wasn't like that before. The program suddenly turned off.These days, it's on the program like the video below. Is there a way to solve this?        

ㅅㄷㄱㄷㄱ.png
LEMON987 by Associate
  • 1171 Views
  • 0 replies
  • 0 kudos