Skip to main content
Associate III
June 26, 2023
Question

stm8s003f

  • June 26, 2023
  • 2 replies
  • 1766 views

Can someone please help me to sort it out?Please 

I am stuck at a project.In the attached code I am unable to wake up the code  after sleep.Rest of the functions working once in sleep it shoild wakeup at if(MV>20)

#include "stm8s.h"
#include "stm8s_clk.h"
#include "stm8s_adc1.h"
#include "stm8s_gpio.h"
#include "stm8s_tim2.h"
#include "main.h"
#include "flash.h"

//#include "stm8s_awu.h"
#include "stm8s_exti.h"




volatile unsigned short _500ms_tick;
volatile unsigned short idle_counter;
volatile uint16_t MV;
void Clk_Config(void);
void ADC_Config(void);
void GPIO_Config(void);
void EXTI_Setup(void);
void ADC_Read1(uint16_t *MV);
void ADC_Read2(uint16_t *Vbat);
void ADC_Read3(uint16_t *Ocd);
void ADC_Read4(uint16_t *Temp);
void EXTI_PortD_Callback(void);




main()
{
uint16_t MV=0,Vbat=0,Ocd=0,Temp=0;
	unsigned short i;
	int counting = 0;


	Clk_Config();
	
	ADC_Config();
	
	GPIO_Config(); 
		

	EXTI_Setup();

	
	
while(MV<100)
	{
		ADC_Read1(&MV);
	 delay_ms(100);
		Set_LED(0);
			idle_counter++;
			 	
		if (idle_counter>=300)
		{
		
		 EnterSleepMode();
		}
	
	
}
						
		

	
	
	
	while (1)
	
	{
	ADC_Read1(&MV);
 delay_ms(100);
		
	ADC_Read2(&Vbat);
	delay_ms(100);
	
	ADC_Read3(&Ocd);
		delay_ms(100);
		
	ADC_Read4(&Temp);
 delay_ms(100);
	
 if (MV > 20) // Mains Detect
			
 
		{
 if ((MV < 370) && (Vbat > 227)) // Mains Fail
					{
 En_Emergency(1); 
						Set_LED(0);
												
					}
			 			
 else 
 {
 En_Emergency(0);
						Set_LED(0);
			 }
				
					
		}
		if(MV<=10)
		{
			ADC_Read3(&Ocd);
			delay_ms(100);
			Set_LED(0);
						if(Ocd<93 || Ocd>186)
						{
						Set_LED(1); 
						delay_ms(1000);	
						Set_LED(0); 
						delay_ms(1000);	
						Set_LED(1); 
						delay_ms(1000);	
						Set_LED(0); 
						delay_ms(1000);	
						Set_LED(1);
						delay_ms(1000);	
						Set_LED(0); 				
				
							delay_ms(5000);	
				
						}
				else if(Ocd>93 || Ocd<186)
				{
				Set_LED(0);
				}
			
			}
	
		ADC_Read2(&Vbat);
			if (MV < 250)
			{
				Set_LED(0);
			}
			if(Vbat>460 || Vbat < 155)
			 {
					Set_Bch(1);
					Set_LED(0);
				}
			else if( Vbat>395)
			 {
					
					Set_LED(1); 
					Set_Bch(0);
				}
			else if(Vbat<383)
				{
						Set_LED(1); 
						Set_Bch(1);
				}
			ADC_Read4(&Temp);
			if(Temp>87 && Temp<425)
			{
				Set_Bch(1);
			}
			else if(Temp<87 || Temp>425)
			{
			 Set_Bch(0);
				Set_LED(1); 
				delay_ms(1000);	
				Set_LED(0); 
				delay_ms(1000);	
				Set_LED(1); 
				delay_ms(1000);	
				Set_LED(0); 
				delay_ms(5000);
			 
			}
		}
			

			
			


}



void Clk_Config() // INTERNAL CLOCK CONFIGUARATION
	{
	CLK_DeInit();
	
	CLK_HSECmd(DISABLE);
	CLK_LSICmd(DISABLE);
	CLK_HSICmd(ENABLE);
	while(CLK_GetFlagStatus(CLK_FLAG_HSIRDY) == FALSE);
	
	CLK_ClockSwitchCmd(ENABLE);
	CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV2);
	CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);
	
	CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSI, 
	DISABLE, CLK_CURRENTCLOCKSTATE_ENABLE);
	

	CLK_PeripheralClockConfig(CLK_PERIPHERAL_ADC, ENABLE);
	 CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, ENABLE);
	}

void ADC_Config() // ADC INITIALIZATION
	{
		 ADC1_DeInit();
		
		 ADC1_Cmd(ENABLE);

 ADC1_ITConfig(ADC1_IT_EOCIE, ENABLE);
		
	}
	
void ADC_Read1(uint16_t *MV)
{
	
	 ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, // MAINS INPUT
					 ADC1_CHANNEL_5,
					 ADC1_PRESSEL_FCPU_D2, 
					 ADC1_EXTTRIG_GPIO, 
					 DISABLE, 
					 ADC1_ALIGN_RIGHT, 
					 ADC1_SCHMITTTRIG_CHANNEL5, 
					 DISABLE);
 ADC1_StartConversion();
 while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
 {
 // Wait for conversion to complete
 }

 *MV= ADC1_GetConversionValue();

}
void ADC_Read2(uint16_t *Vbat)
{
	 ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, //ADC Channel_4 VBATT
					 ADC1_CHANNEL_4,
					 ADC1_PRESSEL_FCPU_D2, 
					 ADC1_EXTTRIG_GPIO, 
					 DISABLE, 
					 ADC1_ALIGN_RIGHT, 
					 ADC1_SCHMITTTRIG_CHANNEL4, 
					 DISABLE);
 ADC1_StartConversion();
 while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
 {
 // Wait for conversion to complete
 }

 
	*Vbat=ADC1_GetConversionValue();
}
void ADC_Read3(uint16_t *Ocd) // ADC Channel_2 OPEN CIRCUIT DETECTION
{
	 ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, 
					 ADC1_CHANNEL_2,
					 ADC1_PRESSEL_FCPU_D2, 
					 ADC1_EXTTRIG_GPIO, 
					 DISABLE, 
					 ADC1_ALIGN_RIGHT, 
					 ADC1_SCHMITTTRIG_CHANNEL2, 
					 DISABLE);
 ADC1_StartConversion();
 while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
 {
 // Wait for conversion to complete
 }

 
	*Ocd=ADC1_GetConversionValue();
}
void ADC_Read4(uint16_t *Temp) // ADC Channel_2 TEMPARATURE MONITORING
{
	 ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, 
					 ADC1_CHANNEL_3,
					 ADC1_PRESSEL_FCPU_D2, 
					 ADC1_EXTTRIG_GPIO, 
					 DISABLE, 
					 ADC1_ALIGN_RIGHT, 
					 ADC1_SCHMITTTRIG_CHANNEL3, 
					 DISABLE);
 ADC1_StartConversion();
 while (!ADC1_GetFlagStatus(ADC1_FLAG_EOC))
 {
 // Wait for conversion to complete
 }

 
	*Temp=ADC1_GetConversionValue();
}

void GPIO_Config(void)
	{
								//GPIO INPUTS
			
		//GPIO_Init(GPIOD,GPIO_PIN_2,GPIO_MODE_IN_FL_NO_IT);			// TEMP SENSE
		GPIO_Init(GPIOD,GPIO_PIN_3,GPIO_MODE_IN_FL_NO_IT);			//VBATT
		GPIO_Init(GPIOD,GPIO_PIN_5,GPIO_MODE_IN_FL_NO_IT);			//MAINS INPUT
		GPIO_Init(GPIOC,GPIO_PIN_4,GPIO_MODE_IN_FL_NO_IT);			// OCD SENSE
		
		
								//GPIO OUTPUTS
								
		GPIO_Init(GPIOA,GPIO_PIN_3,GPIO_MODE_OUT_PP_LOW_FAST);			// MAIN LAMP
		GPIO_Init(GPIOC,GPIO_PIN_3,GPIO_MODE_OUT_PP_HIGH_FAST);			//LED O/P
		GPIO_Init(GPIOC,GPIO_PIN_5,GPIO_MODE_OUT_PP_LOW_FAST);			//BCH
		
	}
void TIM2_Config(void)
{
 TIM2_TimeBaseInit(TIM2_PRESCALER_32768, 244);
 TIM2_ClearFlag(TIM2_FLAG_UPDATE);
 TIM2_ITConfig(TIM2_IT_UPDATE, ENABLE);
 TIM2_Cmd(ENABLE);
		
}


 
INTERRUPT_HANDLER(TIM2_UPD_OVF_BRK_IRQHandler, 13)
{
 if (TIM2_GetITStatus(TIM2_IT_UPDATE) != RESET)
 {
			
 // Increment the idle_counter every 500ms
 idle_counter++;

 // Enter sleep mode if idle for approximately 30 seconds (60 * 500ms)
 if (idle_counter >= 300)
 {
 EnterSleepMode();
 }
				TIM2_ClearITPendingBit(TIM2_IT_UPDATE);
 }
}

void EnterSleepMode(void)
{
 // Disable TIM2 interrupt
 TIM2_ITConfig(TIM2_IT_UPDATE, DISABLE);

 // Disable ADC peripheral
 ADC1_Cmd(DISABLE);

 // Disable GPIO inputs
 GPIO_Init(GPIOD, GPIO_PIN_3, GPIO_MODE_IN_PU_NO_IT);
 GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_IN_FL_IT);
 GPIO_Init(GPIOC, GPIO_PIN_4, GPIO_MODE_IN_PU_NO_IT);

 halt();

 // Re-enable ADC peripheral
 
}

void Inc500mSCounter(void)
{
 if (_500ms_tick < 500)
 {
 _500ms_tick++;
 }
 else
 {
 _500ms_tick = 0;
 idle_counter++;
 }
}
void IWDG_Config(void)
	{
		uint8_t WTG_TIME;
	
		IWDG_Enable();
		
	
		IWDG_WriteAccessCmd(IWDG_WriteAccess_Enable);
		
		
		IWDG_SetPrescaler(IWDG_Prescaler_128);
		
		
		IWDG_SetReload( 127);
		
		
		IWDG_ReloadCounter();
		
	}

void EXTI_Setup(void)
{
	EXTI_DeInit();
	EXTI_SetExtIntSensitivity(EXTI_PORT_GPIOD, EXTI_SENSITIVITY_RISE_ONLY);
	EXTI_SetTLISensitivity(EXTI_TLISENSITIVITY_RISE_ONLY);

}

void WakeupFromSleep(void)
{
	ADC1_Cmd(ENABLE);

 // Re-enable GPIO inputs
 GPIO_Init(GPIOD, GPIO_PIN_3, GPIO_MODE_IN_FL_NO_IT);
 GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_IN_FL_NO_IT);
 GPIO_Init(GPIOC, GPIO_PIN_4, GPIO_MODE_IN_FL_NO_IT);

 // Reset idle counter
 idle_counter = 0;

 // Re-enable TIM2 interrupt
 TIM2_ITConfig(TIM2_IT_UPDATE, ENABLE);
 
}

INTERRUPT_HANDLER(EXTI_PORTD_IRQHandler, 6)
{
	 //EXTI_ClearITPendingBit(EXTI_PORT_GPIOD);
 { // Wake up from sleep mode
 WakeupFromSleep();
 }
}



    This topic has been closed for replies.

    2 replies

    AA1
    Senior III
    June 26, 2023

    As I said before, you should not enter sleep mode in an interrupt handler. In this case in TIM2 interrupt handler. I know that you also call EnterSleepMode() from main, but I don't know which one is executed first.

    And you should not start with a complex program and expect it will work. I believe that you use PD5 pin as the wakeup event. Did you test before and without sleep mode, if this pin generates an interrupt?

    SRAM.11Author
    Associate III
    June 26, 2023

    hi thanks for the reply.I will give a try as what you said .